Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static SeamWeldType |
SeamWeldType.WITH_LASER
Seam weld done by laser
|
static SeamWeldType |
SeamWeldType.WITH_MATERIAL
Seam weld done with material
|
Modifier and Type | Method and Description |
---|---|
SeamWeldType |
SeamWeld.seamWeldType()
Returns the seam weld type
License requirements: None. |
static SeamWeldType |
SeamWeldType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeamWeldType |
SeamWeldType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeamWeldType[] |
SeamWeldType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SeamWeld.setSeamWeldType(SeamWeldType seamWeldType)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.