public class SeamWeldType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_WITH_LASER
Seam weld done by laser
|
static int |
_WITH_MATERIAL
Seam weld done with material
|
static SeamWeldType |
WITH_LASER
Seam weld done by laser
|
static SeamWeldType |
WITH_MATERIAL
Seam weld done with material
|
Modifier and Type | Method and Description |
---|---|
static SeamWeldType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeamWeldType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeamWeldType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SeamWeldType WITH_MATERIAL
public static final SeamWeldType WITH_LASER
public static final int _WITH_MATERIAL
public static final int _WITH_LASER
public static SeamWeldType valueOf(int value)
public static SeamWeldType valueOf(String name)
public static SeamWeldType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.