Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static Dof |
Dof.RX
X Rotation degree of freedom
|
static Dof |
Dof.RY
Y Rotation degree of freedom
|
static Dof |
Dof.RZ
Z Rotation degree of freedom
|
static Dof |
Dof.X
X Translation degree of freedom
|
static Dof |
Dof.Y
Y Translation degree of freedom
|
static Dof |
Dof.Z
Z Translation degree of freedom
|
Modifier and Type | Method and Description |
---|---|
static Dof |
Dof.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Dof |
Dof.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Dof[] |
Dof.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
DofType |
IDof.getDof(Dof dof)
Get the specified degrees of freedom
License requirements: None. |
void |
IDof.setDof(Dof dof,
DofType type)
Set the specified degrees of freedom
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.