Package | Description |
---|---|
nxopen.cae.connections |
Provides classes and interfaces relating to Connections.
|
Modifier and Type | Field and Description |
---|---|
static DofType |
DofType.FIXED
The DOF is fixed
|
static DofType |
DofType.FREE
The DOF is not constrained
|
Modifier and Type | Method and Description |
---|---|
DofType |
IDof.getDof(Dof dof)
Get the specified degrees of freedom
License requirements: None. |
static DofType |
DofType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DofType |
DofType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DofType[] |
DofType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
IDof.setDof(Dof dof,
DofType type)
Set the specified degrees of freedom
License requirements: nx_masterfem ("Finite Element Modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.