Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Class and Description |
---|
AccessorEvaluatorBuilder
Evaluates an object based on a property value or an index
To create a new instance of this class, use AMEManager.createAccessorEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
AccessorEvaluatorBuilder.AccessType
Choices for access type either by an index or property
|
AccessorEvaluatorBuilder.PositionTypeValue
Choices for position to be either begin, end or defined by index
|
AddressObjectIotype
Definition of the Address Object I/O types
See Xml node IoType
|
AMEBaseBuilder
JA class for the insert Eng object dialog
This is an abstract class, and cannot be instantiated. |
AMEBaseNode
Represents Base Node
Use the static method in this class to obtain an instance. |
AMEBaseNode.NodeType
Define the node type
|
AmeDebugSession
Represents a class that is used for AME testing.
|
AmeDebugSession.NavigatorType
Represents type of the navigator
|
AmeDebugSession.ObjectType
Represents type of the object
|
AmeElectricalConnectionPotentialType
Represents electrical connection Pontential Types
|
AMEEngineeringObjectLabel
Represents Engineering Object Label Object
This object does not need a creator. |
AMEEngObject
Represents Engineering Object
This object does not need a creator. |
AMEExtendedObject
Represents Extended Object
Use the static method in this class to obtain an instance. |
AMEGroup
Group Journaling class
This object does not need a creator. |
AMEGroupFolder
Group Folder Journaling class
This object does not need a creator. |
AmeJunctionRepresentationStyleType
Representation style for Tee Junction.
|
AMEManager
Represents a manager of automation designer objects
To obtain an instance of this class, refer to Session Created in NX11.0.0 |
AMEManager.CreateStationType
Type of PLC Station
|
AMEManager.DeleteType
the deletion type
|
AMEManager.PasteObjectsData
This class holds the data returned from
AMEManager.pasteObjects(nxopen.ame.AMEBaseNode) |
AMEManager.PasteStatus
the status of paste operation
|
AmeOpticalConnectionFiberType
Represents optical connection fiber types
|
AMEPort
Represents Port
Use the static method in this class to obtain an instance. |
AMEQuery
The Query Object
This is an abstract class, and cannot be instantiated. |
AmeTeeJunctionType
Represents the type of TeeJunction
|
AmeTeeJunctionVariant
Represents Tee Junction variant index
|
AncestorEvaluatorBuilder
Evaluates an ancestor for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createAncestorEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
AncestorEvaluatorBuilder.JaAspectEvaluatorBuilderNavCriteria
Choices for navigation criteria - Could be By Levels or By Property
|
AncestorEvaluatorBuilder.JaAspectEvaluatorBuilderNavDirection
Choices for direction of navigation - Could be from starting object upwards, or from root node downwards
|
ApplicationBuilder
Create the AD application builder see AMEApplicationBuilder
To create a new instance of this class, use AMEManager.createApplicationBuilder(nxopen.Part) Created in NX11.0.0 |
AspectDetailsBuilder
JA Class for the Aspect Details UI Block
This object does not need a creator. |
AspectNavigatorPreferencesBuilder
JA class for aspect navigator builder
To create a new instance of this class, use AMEManager.createAspectNavigatorPreferencesBuilder(nxopen.Part) Created in NX11.0.0 |
AspectNode
Aspect Node Journaling class
This object does not need a creator. |
AspectPrefixBuilder
represents the builder class which is used to define Aspect Prefixes and Delimiter for
Project To create a new instance of this class, use AMEManager.createAspectPrefixBuilder(nxopen.Part) Created in NX11.0.0 |
AspectPrefixBuilder.DelimiterType
represents delimiter type
|
AssignAspectBuilder
Reassign a single aspect of an Engineering Object
To create a new instance of this class, use AMEManager.createAssignAspectBuilder(nxopen.Part) Created in NX11.0.0 |
AssignSubnetBuilder
Reassign a single aspect of an Engineering Object
To create a new instance of this class, use AMEManager.createAssignSubnetBuilder(nxopen.Part) Created in NX12.0.0 |
AssignTemplateToProductBuilder
Builder class to assign a template object to
ProductDefinition To create a new instance of this class, use AMEManager.createAssignTemplateToProductBuilder(nxopen.ame.ProductDefinition) Created in NX12.0.0 |
AssignTypeBuilder
Builder for selecting an engineering object definition
To create a new instance of this class, use AMEManager.createAssignTypeBuilder(nxopen.Part) Created in NX12.0.0 |
AttributeHolder
JA class for the AttributeHolder object
This is an abstract class, and cannot be instantiated. |
BaseDefinitionAttributeHolder
BaseDefinition Atributes Holder Object
This does not need a creator. |
BaseEvaluatorBuilder
Represents the builder for all the evaluators.
|
BaseEvaluatorBuilder.ConditionType
choices for condition type filter for navigations that return a list of filtered objects
|
BaseEvaluatorBuilder.ContextType
choices for aspect context type, can either be function, location, product, or automation
|
BasicPropertiesBuilder
Represents a re-usable component for basic properties such as name and description
This object does not need a creator. |
BreakTemplateBuilder
JA class for the insert Eng object dialog
To create a new instance of this class, use AMEManager.createBreakTemplateBuilder(nxopen.Part, nxopen.ame.AMEEngObject) Created in NX11.0.0 |
BulkConnectionBuilder
builder for the bulk connection dialog
To create a new instance of this class, use AMEManager.createBulkConnectionBuilder(nxopen.Part) Created in NX11.0.0 |
BulkEngineeringObjectBuilder
BulkEngineeringObjectBuilder class will be used for bulk Engineering Object Operation.
|
BusInterfaceType
Bus Interface type.
|
CabinetComponentNode
Cabinet Component Node class
This object does not need a creator. |
CabinetDesignBuilder
the builder for creating cabinet design
To create a new instance of this class, use AMEManager.createCabinetDesignBuilder(nxopen.Part) Created in NX12.0.0 |
CabinetNode
Cabinet Node class
This object does not need a creator. |
CabinetRoot.CabinetState
Represents cabinet state
|
CallMethodRuleBuilder
JA class for the call method rule dialog
To create a new instance of this class, use AMEManager.createCallMethodRuleBuilder(nxopen.Part, nxopen.ame.PlcCodePosition, nxopen.ame.PlcBlock, nxopen.ame.PlcRule.Type, nxopen.ame.PlcRule.RefObjectType, nxopen.ame.PlcRule.ReplacementType, int, int, int) Created in NX12.0.0 |
CallMethodRuleBuilder.CreationType
replace or insert rule Type
|
ChildrenEvaluatorBuilder
Evaluates the children objects for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createChildrenEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
ChildrenEvaluatorBuilder.FilterType
choices for object type filter, can either be local modules, program blocks, plc data types, or tags
|
ConditionsBuilder
JA class for the conditions dialog .
|
ConfigureResultTableBuilder
Represents configure result table class builder
To create a new instance of this class, use AMEManager.createConfigureResultTableBuilder(nxopen.ame.AMEQuery) Created in NX12.0.0 |
ConnectedObjectsEvaluatorBuilder
Evaluates the connected objects for the given port and a starting point
To create a new instance of this class, use AMEManager.createConnectedObjectsEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
ConnectToLibraryItemBuilder
JA class for the connect to library item dialog
To create a new instance of this class, use AMEManager.connectToLibraryItemBuilder(nxopen.Part, nxopen.ame.InterfaceMemberPort) Created in NX11.0.0 |
ConstantType
The Plc Constant types
|
CreateDefinitionBuilder
Create and classify definition
This object does not need a creator. |
CreateEngObjectDefinitionBuilder
Create and classify engineering object definition
To create a new instance of this class, use AMEManager.createEngObjectDefinitionBuilder(nxopen.Part) Created in NX11.0.0 |
CreatePmiNoteBuilder
Create PMINote dialog JA class
To create a new instance of this class, use AMEManager.createPmiNoteBuilder(nxopen.Part) Created in NX11.0.0 |
CreateProductBuilder
Create and classify product
To create a new instance of this class, use AMEManager.createProductBuilder(nxopen.Part) Created in NX11.0.0 |
CreateTemplateBuilder
Create Template dialog JA class
To create a new instance of this class, use AMEManager.createTemplateBuilder(nxopen.Part) Created in NX11.0.0 |
CreateTemplateDefinitionBuilder
Create and classify template definition
To create a new instance of this class, use AMEManager.createTemplateDefinitionBuilder(nxopen.Part) Created in NX11.0.0 |
DefineAspectBuilder
Define Aspects for Engineering Object Definition
To create a new instance of this class, use AMEManager.defineAspectBuilder(nxopen.Part) Created in NX11.0.0 |
DiagramManager
Represents an object that manages sheet elements.
|
DocumentStructureBuilder
Class to define Document Structure
To create a new instance of this class, use AMEManager.createDocumentStructureBuilder(nxopen.Part) Created in NX11.0.0 |
DocumentType
Represents the type of document
|
EClassNode
EClassData Tree Node class
This object does not need a creator. |
EClassObjectNode
EClassData Tree Node class
This object does not need a creator. |
EditAnnotationBuilder
the builder for creating edit annotation
To create a new instance of this class, use AMEManager.createEditAnnotationBuilder(nxopen.Part, nxopen.ame.AMEExtendedObject) Created in NX12.0.0 |
EditClauseBuilder
Naming Rule Builder
To create a new instance of this class, use AMEManager.createEditClauseBuilder(nxopen.Part, nxopen.ame.AMEQuery, nxopen.ame.QueryClause) Default values. |
EditClauseBuilder.Operator
the query operator
|
EditClauseBuilder.QueryClauseOperatorType
the clause operator
|
EditClauseBuilder.Types
the type of object to be used for edit clause
|
EditEngineeringObjectBuilder
JA class for the Eng object dialog
To create a new instance of this class, use AMEManager.createEditEngineeringObjectBuilder(nxopen.Part, nxopen.ame.AMEEngObject) Created in NX11.0.0 |
EditEngineeringObjectBuilder.SourceType
Assign EOs or POUs
|
EditOrderBuilder
JA class for the Edit Order dialog
To create a new instance of this class, use AMEManager.createEditOrderBuilder(nxopen.Part, nxopen.NXObject) Created in NX12.0.0 |
EditQueryBuilder
Edit Query Builder
To create a new instance of this class, use AMEManager.createEditQueryBuilder(nxopen.Part) Created in NX11.0.0 |
ElectricalAnnotationSettingsBuilder
JA class for the Electrical Annotation Settings dialog
To create a new instance of this class, use AMEManager.createElectricalAnnotationSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
ElectricalAnnotationSettingsBuilder.AnnotationAttrType
Represents the type of annotations
|
ElectricalConnectionSettingsBuilder
Builder object for changing electrical connection settings on diagramming pages associated with the
Project . |
EngineeringObjectAspectDetailBuilder
JA class for the Engineering Object Aspect Detail UI block
.
|
EngineeringObjectAspectDetailBuilder.Columns
Aspect Detail columns
|
EngineeringObjectAspectDetailBuilder.NameSource
Aspect name from
|
EngineeringObjectBaseBuilder
JA class for the insert Eng object dialog
This is an abstract class, and cannot be instantiated. |
EngineeringObjectBuilder
JA class for the insert Eng object dialog
To create a new instance of this class, use AMEManager.createEngineeringObjectBuilder(nxopen.Part) Created in NX11.0.0 |
EngineeringObjectDefinitionLabelBuilder
JA class for the insert Engineering object definition label dialog
To create a new instance of this class, use AMEManager.createEngineeringObjectDefinitionLabelBuilder(nxopen.Part) Created in NX11.0.0 |
EngineeringObjectNameBuilder
JA class for the Engineering Object and Engineering Object def name and description superclass UI block
.
|
EOAttributeHolder
EOAttributeHolder Atributes Holder Object
This does not need a creator. |
EODataItemAttributeHolder
EODef Atributes Holder Object
This does not need a creator. |
EODefAttributeHolder
EODef Atributes Holder Object
This does not need a creator. |
EplanImportProjectTemplateBuilder
EplanImportProjectTemplateBuilder
To create a new instance of this class, use AMEManager.createEplanImportProjectTemplateBuilder(nxopen.Part) Created in NX12.0.0 |
EplanProjectGenerationBuilder
the eplan project generation dialog builder
To create a new instance of this class, use AMEManager.createEplanProjectGenerationBuilder(nxopen.Part) Default values. |
EplanProjectTemplateAndStructureBuilder
JA class for the Eplan project template dialog
To create a new instance of this class, use AMEManager.createEplanProjectTemplateAndStructureBuilder(nxopen.Part) Created in NX12.0.0 |
EplanSettingsBuilder
EplanSettingsBuilder
To create a new instance of this class, use AMEManager.createEplanSettingsBuilder(nxopen.Part, nxopen.ame.AMEBaseNode) Created in NX11.0.0 |
EplanStructureIdentifierOrderBuilder
Represents a Eplan Structure identifier order Builder
To create a new instance of this class, use AMEManager.createEplanStructureIdentifierOrderBuilder(nxopen.Part) Created in NX12.0.0 |
EvaluatorCopyToBuilder
Copies evaluator and its dependents from one engineering object to another
To create a new instance of this class, use AMEManager.createEvaluatorCopyToBuilder(nxopen.Part) Created in NX12.0.0 |
ExportEClassMappingBuilder
Export eclass mapping into file
To create a new instance of this class, use AMEManager.createExportEclassMappingBuilder(nxopen.Part) Created in NX12.0.0 |
ExpressionEvaluator
Represents an Expression Evaluator
This object does not need a creator. |
ExtractAttributeAbsoluteBuilder
Create a extract attribute
This object does not need a creator. |
ExtractAttributeBaseBuilder
Create a extract attribute
This is an abstract class, and cannot be instantiated. |
ExtractAttributeBuilder
Create a extract attribute
To create a new instance of this class, use AMEManager.createExtractAttributeBuilder(nxopen.Part) Created in NX11.0.0 |
ExtractAttributeBuilder.Type
extract type Type
|
ExtractAttributeCurrentObjectBuilder
Create a extract attribute
This object does not need a creator. |
ExtractAttributePortBuilder
Create a extract port attribute builder
This object does not need a creator. |
ExtractAttributeRelativeBuilder
Create a extract attribute
This object does not need a creator. |
FormSheetBuilder
JA class for the Form Sheet dialog
To create a new instance of this class, use AMEManager.createFormSheetBuilder(nxopen.Part, nxopen.ame.FormSheetObject) Default values. |
FormSheetBuilder.SizeOption
Represents form sheet size option
|
FormSheetBuilder.StandardMetricSize
Represents standard metric sizes for form sheet
|
FormSheetObject
JA class for the FormSheetObject
This is an abstract class, and cannot be instantiated. |
FormSheetSettingsBuilder
JA class for the Form Sheet Settings dialog
To create a new instance of this class, use AMEManager.createFormSheetSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
FragmentAttributeHolder
Fragment Object Atributes Holder
This does not need a creator. |
FragmentBuilder
Represents a Fragment creation class Builder
To create a new instance of this class, use AMEManager.createFragmentBuilder(nxopen.Part) Created in NX11.0.0 |
FragmentObject
Represents a Fragment Object
This object does not need a creator. |
FunctionCallInstanceBuilder
JA class for the reuse rule dialog
To create a new instance of this class, use AMEManager.createFunctionCallInstanceBuilder(nxopen.Part, nxopen.ame.PlcBlock) Created in NX12.0.0 |
GeneralAnnotationSettingsBuilder
builder for the general annotation settings dialog
To create a new instance of this class, use AMEManager.createGeneralAnnotationSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
GeneralAnnotationSettingsBuilder.AnnotationSeparator
the separator for annotation set
|
GeneralAnnotationSettingsBuilder.HorizontalTextPosition
horizontal text postion type
|
GeneralAnnotationSettingsBuilder.SourceAndTargetSeparator
the separator between Source and Target
|
GeneralAnnotationSettingsBuilder.VerticalTextPosition
verical text postion type
|
GeneralConnectionSettingsBuilder
Builder for the General Connection Settings dialog
To create a new instance of this class, use AMEManager.createGeneralConnectionSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
GenerateReportsBuilder
Comment
To create a new instance of this class, use AMEManager.createGenerateReportsBuilder(nxopen.Part) Created in NX11.0.0 |
GlobalSelectionBuilder
GlobalSelectionBuilder
To create a new instance of this class, use AMEManager.createGlobalSelectionBuilder(nxopen.Part) Created in NX11.0.0 |
GroupBuilder
JA class for groups
To create a new instance of this class, use AMEManager.createGroupBuilder(nxopen.Part, nxopen.ame.AMEGroup) Created in NX11.0.0 |
IEngObject
Represents Engineering Object .
|
ImportEClassMappingBuilder
Import eClass mapping
To create a new instance of this class, use AMEManager.createImportEclassMappingBuilder(nxopen.Part) Created in NX12.0.0 |
ImportEclassMappingMode
enum for import eClass mapping mode.
|
ImportEClassProductBuilder
Imports a eclass product xml file
To create a new instance of this class, use AMEManager.createImportEclassProductBuilder(nxopen.Part) Created in NX12.0.0 |
ImportEClassSchemaBuilder
Imports a eclass schema xml file
To create a new instance of this class, use AMEManager.createImportEclassSchemaBuilder(nxopen.Part) Created in NX12.0.0 |
ImportEplanPageMacroBuilder
ImportEplanPageMacroBuilder
To create a new instance of this class, use AMEManager.createImportEplanPageMacroBuilder(nxopen.Part) Created in NX11.0.0 |
ImportGlobalMappingBuilder
Imports a global mapping xml file
To create a new instance of this class, use AMEManager.createImportGlobalMappingBuilder(nxopen.Part) Created in NX12.0.0 |
ImportHWXmlBuilder
the Import HW Xml builder
To create a new instance of this class, use AMEManager.createImportHwxmlBuilder(nxopen.Part, nxopen.ame.AMEBaseNode) Created in NX11.0.0 |
ImportNode
Import Object Journaling class
This object does not need a creator. |
ImportType
Definition of the EClass mapping behaviour types
|
InsertObjectBuilder
JA class for Insert Object dialog
To create a new instance of this class, use AMEManager.createInsertObjectBuilder(nxopen.Part) Created in NX12.0.0 |
InsertSettingsBuilder
Re-usable UI for Settings properties in Insert EO and Insert Template dialog .
|
InstanceDataBlockBuilder
JA class for the reuse rule dialog
To create a new instance of this class, use AMEManager.createInstanceDataBlockBuilder(nxopen.Part, nxopen.ame.PlcBlock, nxopen.ame.InstanceDataBlockBuilder.CreateMode) Created in NX11.0.0 |
InstanceDataBlockBuilder.ActionType
the idb scope
|
InstanceDataBlockBuilder.CreateMode
the idb create mode
|
InstantiateBaseDefinitionReuseSelectionBuilder
Builder for selecting base definition
this is a block . |
InstantiateTemplateBulkBuilder
JA class for the insert Eng object dialog
To create a new instance of this class, use AMEManager.createInstantiateTemplateBulkBuilder(nxopen.Part, java.lang.String) Default values. |
InstantiateTemplateBulkBuilder.PlacementType
Choices for placement type, can be Place in Navigator or Place on Page
|
InterfaceAccessType
The Plc Interface Access types
|
InterfaceMemberPort
InterfaceMemberPort Journaling class
This object does not need a creator. |
InterruptionPointBuilder
Represents builder for AME::DB::InterruptionPoint
To create a new instance of this class, use AMEManager.createInterruptionPointBuilder(nxopen.Part, nxopen.ame.AMEExtendedObject) Created in NX12.0.0 |
InterruptionPointBuilder.Variant
Represents Interruption Point Variant type
|
IPort
Represents an IPort
This is an abstract class, and cannot be instantiated. |
LayoutDefinitionBuilder
interface for the LayoutDefinitionBuilder
To create a new instance of this class, use AMEManager.createLayoutDefinitionBuilder(nxopen.Part) Created in NX11.0.0 |
LineDesignerMappingBuilder
Line Designer mapping dialog JA interface
To create a new instance of this class, use AMEManager.createLineDesignerMappingBuilder(nxopen.Part) Default values. |
LineDesignerMappingBuilder.FilterType
enum for the filter
|
LinkSymbolToDeviceTypeBuilder
JA class for LinkSymbolToDeviceTypeBuilder dialog
To create a new instance of this class, use AMEManager.createLinkSymbolToDeviceTypeBuilder(nxopen.Part) Created in NX11.0.0 |
LoadLineDesignerBuilder
JA class for the insert LoadLineDesigner dialog
To create a new instance of this class, use AMEManager.createLoadLineDesignerBuilder(nxopen.Part) Created in NX11.0.0 |
LoadLineDesignerBuilder.RevisionRuleType
enum for the revision rule
|
Manage2dSymbolsBuilder
Represents a Manage2dSymbolsBuilder class Builder
To create a new instance of this class, use AMEManager.createManage2dSymbolsBuilder(nxopen.Part) Default values. |
Manage2dSymbolsBuilder.SymbolRepresentationTypes
Representation type of symbol
|
Manage3DModelsBuilder
Represents the builder that is used to assign 3D models to a
ProductDefinition
To create a new instance of this class, use AMEManager.createManage3dmodelsBuilder(nxopen.Part) Created in NX11.0.0 |
ManageEclassMappingBuilder
Represents a ManageEclassMappingBuilder class Builder
To create a new instance of this class, use AMEManager.createManageEclassmappingBuilder(nxopen.Part) Created in NX11.0.0 |
ManageObjectTypeBuilder
Builder class for assigning AD type to
Part and name to Component To create a new instance of this class, use AMEManager.createManageObjectTypeBuilder(nxopen.Part) Created in NX12.0.0 |
MapToExistingObjectBuilder
Line Designer map to existing (EO) dialog JA interface
To create a new instance of this class, use AMEManager.createMapToExistingObjectBuilder(nxopen.Part) Created in NX11.0.0 |
MemorySectionType
Definition of the memory section types
|
MountingInterfaceBuilder
Builder class for creating mounting interface object in
Part To create a new instance of this class, use AMEManager.createMountingInterfaceBuilder(nxopen.Part) Default values. |
MountingInterfaceBuilder.FixingPolicy
Represents component fixing type
|
MountingInterfaceBuilder.InterfaceType
Represents mounting interface type
|
MountingInterfaceBuilder.ReceptaclePolicy
Represents component receptacle type
|
MultipleObjectsBuilder
JA class for the insert Eng object dialog
This is an abstract class, and cannot be instantiated. |
MultiValueObjectsPort
MultiValueObjectsPort Journaling class
This object does not need a creator. |
MultiValueObjectsPort.JaAmeValueObjectUsageType
type which usagetype has to be used
|
NamingRuleBuilder
Naming Rule Builder
To create a new instance of this class, use NamingRuleListBuilder.createRule() Created in NX11.0.0 |
NamingRuleBuilderList
Represents a list of objects.
|
NamingRuleListBuilder
Classification to Engineering Object Name Map Builder
this is a block . |
NamingRuleSettingsBuilder
JA class for dialog for naming rule settings
To create a new instance of this class, use AMEManager.createNamingRuleSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
NamingRuleSettingsBuilder.Sources
different types of Delimiter sources
|
ObjectConnectionBuilder
JA class for the reuse object connection block .
|
ObjectConnectionDetailBuilder
JA class for the reuse object connection detail block .
|
ObjectEvaluatorBuilder
Evaluates the object given a starting point
To create a new instance of this class, use AMEManager.createObjectEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
ObjectNameBuilder
Object Name JA class .
|
ObjectNameIndexBuilder
Object Name Index JA class .
|
OperandRuleBuilder
JA class for the parameter rule dialog
To create a new instance of this class, use AMEManager.createOperandRuleBuilder(nxopen.Part, nxopen.ame.PlcCodePosition, nxopen.ame.PlcBlock, int, int, nxopen.ame.PlcRule.Type) Created in NX11.0.0 |
OperandRuleBuilder.CreationType
replace or insert rule Type
|
OperatorRuleBuilder
OperatorRule Dialog
To create a new instance of this class, use AMEManager.createOperatorRuleBuilder(nxopen.Part, nxopen.ame.PlcCodePosition, nxopen.ame.PlcBlock, nxopen.ame.PlcRule.Type, nxopen.ame.PlcRule.RefObjectType, nxopen.ame.PlcRule.ReplacementType, int, int, int) Created in NX12.0.0 |
OperatorRuleBuilder.NegationValue
Enum of negation value
|
OperatorRuleBuilder.ParameterType
Enum of parameter type
|
OpticalAnnotationSettingsBuilder
JA class for the Optical Annotation Settings dialog
To create a new instance of this class, use AMEManager.createOpticalAnnotationSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
OpticalAnnotationSettingsBuilder.AnnotationAttrType
Represents the type of annotations
|
OpticalConnectionSettingsBuilder
Builder object for changing optical connection settings on diagramming pages associated with the
Project To create a new instance of this class, use AMEManager.createOpticalConnectionSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
OrderAspectsBuilder
Represents a
OrderAspectsBuilder for changing the order of Navigator
To create a new instance of this class, use AMEManager.createOrderAspectsBuilder(nxopen.Part) Created in NX11.0.0 |
OrderAspectsBuilder.OrderType
possible choices for order of navigator objects
|
OrderAspectsBuilder.SortType
possible choices for sorting of navigator objects in a set
|
PageAttributeHolder
Page Object Atributes Holder
This does not need a creator. |
PageBuilder
Represents a Page creation class Builder
To create a new instance of this class, use AMEManager.createPageBuilder(nxopen.Part) Default values. |
PageBuilder.Types
Represents the type of page
|
PageNamingBuilder
Class to define Page naming schema
To create a new instance of this class, use AMEManager.createPageNamingBuilder(nxopen.Part) Default values. |
PageObject
Represents a Page Object
This object does not need a creator. |
ParameterRuleBuilder
JA class for the parameter rule dialog
To create a new instance of this class, use AMEManager.createParameterRuleBuilder(nxopen.Part, nxopen.ame.MultiValueObjectsPort, nxopen.ame.PlcRule.Type, nxopen.ame.MultiValueObjectsPort.JaAmeValueObjectUsageType) Created in NX12.0.0 |
ParameterRuleBuilder.Connection
connection Type
|
ParentEvaluatorBuilder
Evaluates the parent object for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createParentEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
PlaceAutomationBuilder
Reassign a single aspect of an Engineering Object
To create a new instance of this class, use AMEManager.createPlaceAutomationBuilder(nxopen.Part) Created in NX12.0.0 |
PlcBlock
Plc Block Node Journaling class
This is an abstract class. |
PlcCodePosition
Represents Plc Code Position Object
This object does not need a creator. |
PlcDataType
Definition of the PLC data types
|
PlcDataTypeSource
Definition of the data type sources
|
PlcMemoryAreaBuilder
Represents a Subnet creation class Builder
To create a new instance of this class, use AMEManager.createPlcMemoryAreaBuilder(nxopen.Part, nxopen.ame.AMEBaseNode) Created in NX12.0.0 |
PlcMethod
Plc Method Node Journaling class
This is an abstract class. |
PlcMethodBuilder
The Journalling class for PlcMethodBuilder
To create a new instance of this class, use AMEManager.createPlcMethodBuilder(nxopen.Part, nxopen.ame.PlcMethod) Created in NX11.0.0 |
PlcRule.RefObjectType
type which discribed the context object
|
PlcRule.ReplacementType
type which defined wich object has to be replaced
|
PlcRule.Type
replace or insert rule Type.
|
PlcSoftwareGenPort
PlcSoftwareGenPort Journaling class
This object does not need a creator. |
PlcSymbolBuilder
Class to create Functional Tags and assign them to PLC Channels
To create a new instance of this class, use AMEManager.createPlcSymbolBuilder(nxopen.Part, nxopen.ame.AMEBaseNode) Created in NX11.0.0 |
PlcSymbolsEvaluatorBuilder
Evaluates the PLC tags for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createPlcSymbolsEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
PlcSymbolsEvaluatorBuilder.FilterType
choices for type filter, can either be tags, instance dbs, function blocks, functions, eplan macros, or all
|
PlcVendorSymbolBuilder
Represents a Subnet creation class Builder
To create a new instance of this class, use AMEManager.createPlcVendorSymbolBuilder(nxopen.Part, nxopen.NXObject) Created in NX12.0.0 |
PortAttributeHolder
Port Object Atributes Holder
This does not need a creator. |
PortBuilder
builder for the software block properties dialog
To create a new instance of this class, use AMEManager.createPortBuilder(nxopen.Part, nxopen.NXObject, nxopen.NXObject) Created in NX11.0.0 |
PortBuilder.ConnectableAttrProxyObjectType
Represents the type of connectable attribute proxy object for typed port
|
PortBuilder.CreationModeType
Represents the type of creation mode
|
PortBuilder.Type
the type of a port
|
PortConnectionBuilder
builder for the port connector dialog
To create a new instance of this class, use AMEManager.createPortConnectionBuilder(nxopen.Part, nxopen.NXObject) Created in NX11.0.0 |
PortEvaluatorBuilder
Evaluates the port objects for the given port and a starting point
To create a new instance of this class, use AMEManager.createPortEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
PortsManagerBuilder
Provides journal methods for the ports manager dialog.
|
ProductComponent
Product Component class
This object does not need a creator. |
ProductComponentInstance
Product Component Instance class
This object does not need a creator. |
ProductDefAttributeHolder
ProductDefinition Atributes Holder Object
This does not need a creator. |
ProductDefinition
JA class for the Product Definition object
This is an abstract class, and cannot be instantiated. |
ProductMatchingRulesBuilder
Represents Product Matching Rules class builder
To create a new instance of this class, use AMEManager.createProductMatchingRulesBuilder(nxopen.Part) Created in NX11.0.0 |
ProductMatchingRulesBuilder.Condition
Represents matching rule condition
|
ProductSelectionBuilder
JA class for Product Selection dialog
To create a new instance of this class, use AMEManager.createProductSelectionBuilder(nxopen.Part) Default values. |
ProductSelectionBuilder.Type
the product type for product selection
|
ProductSelectionDetailsBuilder
Represents a Product Selection Details class Builder
To create a new instance of this class, use AMEManager.createProductSelectionDetailsBuilder(nxopen.Part) Created in NX11.0.0 |
ProgrammingLanguage
The Plc Programming Languages
|
Project
Project Journaling class
Created by Application_AME_ApplicationBuilder when we enter the application . |
ProjectEngineeringObjectBuilder
JA class for the insert Project Eng object dialog
To create a new instance of this class, use AMEManager.createProjectEngineeringObjectBuilder(nxopen.Part) Created in NX11.0.0 |
PropertyEvaluatorBuilder
Evaluates the property of an object given a category and property
To create a new instance of this class, use AMEManager.createPropertyEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
QueryBuilder
Represents query class builder
To create a new instance of this class, use AMEManager.createQueryBuilder(nxopen.Part) Created in NX11.0.0 |
QueryBuilder.Types
the creation type of query
|
QueryClause
JA class for the QueryClause object
This is an abstract class, and cannot be instantiated. |
QueryFolder
Query Folder Journaling class
This object does not need a creator. |
ReferenceObjectBuilder
Re-usable UI consist of a context and source selection .
|
ReferenceObjectBuilder.SourceSelectionType
possible choices for source object selection
|
ReportsSettingsBuilder
interface for the ReportsSettingsBuilder
To create a new instance of this class, use AMEManager.createReportsSettingsBuilder(nxopen.Part) Created in NX11.0.0 |
ReportTemplateBuilder
Class to create Report Template and assign the ReportQuery and Report Layout to them
To create a new instance of this class, use AMEManager.createReportTemplateBuilder(nxopen.Part) Created in NX11.0.0 |
SaveToLibraryBuilder
Create Software Block JA class
To create a new instance of this class, use AMEManager.createSaveToLibraryBuilder(nxopen.Part) Created in NX11.0.0 |
SchematicSymbolConfigurationBuilder
JA class for SchematicSymbolConfigurationBuilder dialog
To create a new instance of this class, use AMEManager.createSchematicSymbolConfigurationBuilder(nxopen.Part) Created in NX11.0.0 |
SelectAMEBaseNode
Represents a single object selection.
|
SelectAMEBaseNode.ValueData
This class holds the data returned from
SelectAMEBaseNode.getValue() |
SelectAMEBaseNode.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectAMEBaseNode.getValue() |
SelectAMEBaseNode.ValueWithSnapData
This class holds the data returned from
SelectAMEBaseNode.getValue() |
SelectAMEBaseNodeList
Represents a list of objects on a selection list.
|
SelectAMEExtendedObject
Represents a single object selection.
|
SelectAMEExtendedObject.ValueData
This class holds the data returned from
SelectAMEExtendedObject.getValue() |
SelectAMEExtendedObject.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectAMEExtendedObject.getValue() |
SelectAMEExtendedObject.ValueWithSnapData
This class holds the data returned from
SelectAMEExtendedObject.getValue() |
SelectAMEPort
Represents a single object selection.
|
SelectAMEPort.ValueData
This class holds the data returned from
SelectAMEPort.getValue() |
SelectAMEPort.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectAMEPort.getValue() |
SelectAMEPort.ValueWithSnapData
This class holds the data returned from
SelectAMEPort.getValue() |
SelectAndHighlightBuilder
Represents a
SelectAndHighlightBuilder for select and highlight in the Navigators
To create a new instance of this class, use AMEManager.selectAndHighlightBuilder(nxopen.Part) Created in NX11.0.0 |
SelectAndHighlightBuilder.SelType
possible choices for selecting of navigator objects in a set
|
SelectAspectNode
Represents a single object selection.
|
SelectAspectNode.ValueData
This class holds the data returned from
SelectAspectNode.getValue() |
SelectAspectNode.ValueWithCaeSetObjectInfoData
This class holds the data returned from
SelectAspectNode.getValue() |
SelectAspectNode.ValueWithSnapData
This class holds the data returned from
SelectAspectNode.getValue() |
SelectBaseDefinitionNodeBuilder
Builder for selecting base definition node from navigators
This object does not need a creator . |
SelectClassificationBuilder
Select a part from the reuse library .
|
SelectClassificationFromTreeBuilder
Select Type from the Classification Library
This object does not need a creator. |
SelectionBaseDefinitionBuilder
Journalling Interface class for Builder which allows selection of BaseDefinition.
|
SelectionEngineeringObjectDefinitionBuilder
JA class for the Engineering Object Definition Block
This object does not need a creator. |
SelectMountingInterfaceLocationBuilder
Builder for selecting mounting interface location from graphics window
This object does not need a creator . |
SelectProductOrEoDefinitionBuilder
JA class for the Product Definition or Engineering Object Definition Selection
This object does not need a creator. |
ShowHideObjectsBuilder
JA class for ShowHideObjectsBuilder
To create a new instance of this class, use AMEManager.createShowHideObjectsBuilder(nxopen.Part) Created in NX11.0.0 |
Snap3DModelsBuilder
Represents a Snap3DModelsBuilder class Builder
To create a new instance of this class, use AMEManager.createSnap3dmodelsBuilder(nxopen.Part) Created in NX12.0.0 |
SortingBlockBuilder
Sorts the list expression output according to the property .
|
SortingBlockBuilder.Order
possible choices for order selection
|
SubnetBuilder
Represents a Subnet creation class Builder
To create a new instance of this class, use AMEManager.createSubnetBuilder(nxopen.Part) Created in NX12.0.0 |
SymbolAnnotationBuilder
Represents a Symbol Annotation creation class Builder
To create a new instance of this class, use AMEManager.createSymbolAnnotationBuilder(nxopen.Part) Created in NX12.0.0 |
SymbolAnnotationBuilder.Anchor
Represents anchor of annotation
|
SymbolAnnotationBuilder.Orientation
Represents orientation of annotation
|
SymbolAnnotationSettingsBuilder
JA class for the symbol settings
To create a new instance of this class, use AMEManager.createSymbolAnnotationSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
SymbolAuthoringBuilder
Represents a Symbol Authoring class Builder
To create a new instance of this class, use AMEManager.createSymbolAuthoringBuilder(nxopen.Part) Default values. |
SymbolAuthoringBuilder.Types
Represents the type of symbol
|
TCSavedQueriesBuilder
Represents a TC Saved Queries builder
To create a new instance of this class, use AMEManager.createEditQueryScopeBuilder(nxopen.Part, nxopen.ame.AMEQuery, nxopen.ame.QueryClause) Created in NX11.0.0 |
TeeJunctionBuilder
JA class for creating Tee Junction
To create a new instance of this class, use AMEManager.createTeeJunctionBuilder(nxopen.Part) Created in NX12.0.0 |
TiaPortalProjectSettingsBuilder
TiaPortalProjectSettingsBuilder
To create a new instance of this class, use AMEManager.createTiaPortalProjectSettingsBuilder(nxopen.Part) Created in NX12.0.0 |
TiaPortalProjectSettingsBuilder.TiaPortalVersionType
represents TIA Portal Version type
|
TiaProjectItemBuilder
the TIA project item builder
To create a new instance of this class, use AMEManager.createTiaprojectItemBuilder(nxopen.Part) Created in NX11.0.0 |
TransferFileDataBuilder
Imports a new one or updates the existing configuration in AD Upstream Data Navigator from the external file.
|
TypeMappingBuilder
JA class for the type mapping dialog
this is a block . |
TypeMappingBuilder.LoadData
This class holds the data returned from
TypeMappingBuilder.load(java.lang.String) |
TypeMappingBuilderList
Represents a list of objects.
|
TypeMappingListBuilder
Type Mapping List Builder
To create a new instance of this class, use AMEManager.createTypeMappingListBuilder(nxopen.Part) Created in NX11.0.0 |
UnloadLineDesignerBuilder
JA class for the insert UnloadLineDesigner dialog
To create a new instance of this class, use AMEManager.createUnloadLineDesignerBuilder(nxopen.Part) Created in NX11.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.