Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Field and Description |
---|---|
static AmeTeeJunctionType |
AmeTeeJunctionType.HORIZONTAL_DOWN |
static AmeTeeJunctionType |
AmeTeeJunctionType.HORIZONTAL_UP |
static AmeTeeJunctionType |
AmeTeeJunctionType.INVALID |
static AmeTeeJunctionType |
AmeTeeJunctionType.VERTICAL_LEFT |
static AmeTeeJunctionType |
AmeTeeJunctionType.VERTICAL_RIGHT |
Modifier and Type | Method and Description |
---|---|
static AmeTeeJunctionType |
AmeTeeJunctionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AmeTeeJunctionType |
AmeTeeJunctionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AmeTeeJunctionType[] |
AmeTeeJunctionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TeeJunctionBuilder.setTeeJunctionType(AmeTeeJunctionType junctionType)
Set TeeJunction type.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.