Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BulkEngineeringObjectBuilder
BulkEngineeringObjectBuilder class will be used for bulk Engineering Object Operation.
|
interface |
EngineeringObjectBaseBuilder
JA class for the insert Eng object dialog
This is an abstract class, and cannot be instantiated. |
interface |
EngineeringObjectBuilder
JA class for the insert Eng object dialog
To create a new instance of this class, use AMEManager.createEngineeringObjectBuilder(nxopen.Part) Created in NX11.0.0 |
interface |
InstantiateTemplateBulkBuilder
JA class for the insert Eng object dialog
To create a new instance of this class, use AMEManager.createInstantiateTemplateBulkBuilder(nxopen.Part, java.lang.String) Default values. |
interface |
PageBuilder
Represents a Page creation class Builder
To create a new instance of this class, use AMEManager.createPageBuilder(nxopen.Part) Default values. |
interface |
ProjectEngineeringObjectBuilder
JA class for the insert Project Eng object dialog
To create a new instance of this class, use AMEManager.createProjectEngineeringObjectBuilder(nxopen.Part) Created in NX11.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.