Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Method and Description |
---|---|
SelectClassificationFromTreeBuilder |
CreateProductBuilder.selectClassificationFromTree()
Deprecated.
Deprecated in NX12.0.0. The newly created product is placed under the product library node which corresponds to the Type Library path of the selected Device Type. If the selected type has no counterpart in the Product structure, system automatically places those directly under Device Product Library node.
|
SelectClassificationFromTreeBuilder |
CreateDefinitionBuilder.selectClassificationFromTree()
Returns the select classification from tree builder
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.