public interface CreateProductBuilder extends Builder
AMEManager.createProductBuilder(nxopen.Part)
Modifier and Type | Method and Description |
---|---|
NXObject |
createTypeAttribute()
Creates a new type attribute object
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
SelectClassificationFromTreeBuilder |
selectClassificationFromTree()
Deprecated.
Deprecated in NX12.0.0. The newly created product is placed under the product library node which corresponds to the Type Library path of the selected Device Type. If the selected type has no counterpart in the Product structure, system automatically places those directly under Device Product Library node.
|
SelectionEngineeringObjectDefinitionBuilder |
selectionEngObjectDefinition()
Returns the engineering object definition
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
void |
setObjectNameOnTypeAttr()
Sets the Object Name on Type Attribute Object.
|
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
SelectionEngineeringObjectDefinitionBuilder selectionEngObjectDefinition() throws NXException, RemoteException
NXException
RemoteException
SelectClassificationFromTreeBuilder selectClassificationFromTree() throws NXException, RemoteException
NXException
RemoteException
NXObject createTypeAttribute() throws NXException, RemoteException
NXException
RemoteException
void setObjectNameOnTypeAttr() throws NXException, RemoteException
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.