Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Field and Description |
---|---|
static EditClauseBuilder.Types |
EditClauseBuilder.Types.ASPECT |
static EditClauseBuilder.Types |
EditClauseBuilder.Types.CLASSIFICATION |
static EditClauseBuilder.Types |
EditClauseBuilder.Types.LIBRARY_OBJECT |
Modifier and Type | Method and Description |
---|---|
EditClauseBuilder.Types |
EditClauseBuilder.type()
Returns the type of object to be used for edit clause
EditClauseBuilder.type()
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") Created in NX11.0.0 |
static EditClauseBuilder.Types |
EditClauseBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EditClauseBuilder.Types |
EditClauseBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EditClauseBuilder.Types[] |
EditClauseBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EditClauseBuilder.setType(EditClauseBuilder.Types type)
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.