Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AccessorEvaluatorBuilder
Evaluates an object based on a property value or an index
To create a new instance of this class, use AMEManager.createAccessorEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
interface |
AncestorEvaluatorBuilder
Evaluates an ancestor for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createAncestorEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
interface |
ChildrenEvaluatorBuilder
Evaluates the children objects for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createChildrenEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
interface |
ConnectedObjectsEvaluatorBuilder
Evaluates the connected objects for the given port and a starting point
To create a new instance of this class, use AMEManager.createConnectedObjectsEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
interface |
ObjectEvaluatorBuilder
Evaluates the object given a starting point
To create a new instance of this class, use AMEManager.createObjectEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
interface |
ParentEvaluatorBuilder
Evaluates the parent object for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createParentEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
interface |
PlcSymbolsEvaluatorBuilder
Evaluates the PLC tags for a given aspect and a starting point
To create a new instance of this class, use AMEManager.createPlcSymbolsEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
interface |
PortEvaluatorBuilder
Evaluates the port objects for the given port and a starting point
To create a new instance of this class, use AMEManager.createPortEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
interface |
PropertyEvaluatorBuilder
Evaluates the property of an object given a category and property
To create a new instance of this class, use AMEManager.createPropertyEvaluatorBuilder(nxopen.Part, nxopen.ame.ExpressionEvaluator) Created in NX12.0.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.