Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Method and Description |
---|---|
TypeMappingBuilder |
TypeMappingListBuilder.createTypeMapping()
Create a new type mapping
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
TypeMappingBuilder |
TypeMappingBuilderList.findItem(int index)
Returns the object at the input index.
|
TypeMappingBuilder[] |
TypeMappingBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
TypeMappingBuilder[] |
TypeMappingListBuilder.loadAd(String adPath)
Loads the Ld types linked to the given AD type
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
TypeMappingBuilder[] |
TypeMappingListBuilder.loadAllLdTypes()
Loads the Ld types in the project
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
Modifier and Type | Method and Description |
---|---|
void |
TypeMappingBuilderList.append(TypeMappingBuilder object)
Appends an object to the list
License requirements: None. |
void |
TypeMappingBuilderList.append(TypeMappingBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
TypeMappingListBuilder.deleteTypeMapping(TypeMappingBuilder mappingBuilder)
Delete type mapping
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
void |
TypeMappingBuilderList.erase(TypeMappingBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
TypeMappingBuilderList.erase(TypeMappingBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
TypeMappingBuilderList.findIndex(TypeMappingBuilder obj)
Finds the index where the input object appears.
|
void |
TypeMappingBuilderList.insert(int location,
TypeMappingBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
TypeMappingBuilderList.setContents(TypeMappingBuilder[] objects)
Sets the contents of the entire list.
|
void |
TypeMappingBuilderList.swap(TypeMappingBuilder object1,
TypeMappingBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.