Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Field and Description |
---|---|
static MountingInterfaceBuilder.InterfaceType |
MountingInterfaceBuilder.InterfaceType.COMPONENT_RECEPTACLE |
static MountingInterfaceBuilder.InterfaceType |
MountingInterfaceBuilder.InterfaceType.FIXING |
Modifier and Type | Method and Description |
---|---|
MountingInterfaceBuilder.InterfaceType |
MountingInterfaceBuilder.mountingInterfaceType()
Returns the
MountingInterfaceBuilder.InterfaceType
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") Created in NX12.0.0 |
static MountingInterfaceBuilder.InterfaceType |
MountingInterfaceBuilder.InterfaceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MountingInterfaceBuilder.InterfaceType |
MountingInterfaceBuilder.InterfaceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MountingInterfaceBuilder.InterfaceType[] |
MountingInterfaceBuilder.InterfaceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MountingInterfaceBuilder.setMountingInterfaceType(MountingInterfaceBuilder.InterfaceType type)
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.