Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AMEPort
Represents Port
Use the static method in this class to obtain an instance. |
interface |
AssignmentPort
Represents AssignmentPort
Use the static method in this class to obtain an instance. |
interface |
EPLANPlug
Represents EPLANPlug
Use the static method in this class to obtain an instance. |
interface |
EPLANSocket
Represents EPLANSocket
Use the static method in this class to obtain an instance. |
interface |
InterfaceMemberPort
InterfaceMemberPort Journaling class
This object does not need a creator. |
interface |
MultiValueObjectsPort
MultiValueObjectsPort Journaling class
This object does not need a creator. |
interface |
PlcSoftwareGenPort
PlcSoftwareGenPort Journaling class
This object does not need a creator. |
Modifier and Type | Method and Description |
---|---|
void |
BulkConnectionBuilder.disconnect(IPort[] sourcePorts,
IPort[] targetPorts)
Disconnect the Connections
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
void |
BulkConnectionBuilder.disconnect(IPort[] sourcePorts,
IPort[] targetPorts)
Disconnect the Connections
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.