Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Interface and Description |
---|---|
interface |
AMEPort
Represents Port
Use the static method in this class to obtain an instance. |
interface |
AssignmentPort
Represents AssignmentPort
Use the static method in this class to obtain an instance. |
interface |
EPLANPlug
Represents EPLANPlug
Use the static method in this class to obtain an instance. |
interface |
EPLANSocket
Represents EPLANSocket
Use the static method in this class to obtain an instance. |
interface |
InterfaceMemberPort
InterfaceMemberPort Journaling class
This object does not need a creator. |
interface |
MultiValueObjectsPort
MultiValueObjectsPort Journaling class
This object does not need a creator. |
interface |
PlcMethod
Plc Method Node Journaling class
This is an abstract class. |
interface |
PlcSoftwareGenPort
PlcSoftwareGenPort Journaling class
This object does not need a creator. |
Modifier and Type | Field and Description |
---|---|
AMEExtendedObject |
SelectAMEExtendedObject.ValueData.selection
selected object
|
AMEExtendedObject |
SelectAMEExtendedObject.ValueWithCaeSetObjectInfoData.selection
selected object
|
AMEExtendedObject |
SelectAMEExtendedObject.ValueWithSnapData.selection1
first selected object
|
AMEExtendedObject |
SelectAMEExtendedObject.ValueWithSnapData.selection2
second selected object
|
Modifier and Type | Method and Description |
---|---|
AMEExtendedObject |
SelectAMEExtendedObject.value()
Returns the object being selected
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
Connection |
DiagramManager.createConnection(Sheet sheet,
AMEExtendedObject startPort,
AMEExtendedObject endPort,
Point2d[] p2dBendPoints)
Create Diagramming Connection
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
EditAnnotationBuilder |
AMEManager.createEditAnnotationBuilder(Part part,
AMEExtendedObject extObject)
Creates a
EditAnnotationBuilder
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") Created in NX12.0.0 |
InterruptionPointBuilder |
AMEManager.createInterruptionPointBuilder(Part part,
AMEExtendedObject interruptionPoint)
Creates a
InterruptionPointBuilder
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") Created in NX12.0.0 |
void |
DiagramManager.reconnectConnection(Sheet sheet,
Connection connection,
AMEExtendedObject targetPort,
int connectionLocationType)
Reconnect Diagramming Connection
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
void |
TeeJunctionBuilder.setContextConnectionPortAndBendPoints(AMEExtendedObject contextConnectionPort,
Point2d[] p2dBendPoints)
Set Context Connection's Start Port and it's Bend Points.
|
void |
InterruptionPointBuilder.setDestinationInterruptionPoint(AMEExtendedObject interruptionPoint)
Set the destination interruption point to link to
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
void |
SelectAMEExtendedObject.setValue(AMEExtendedObject selection)
Sets the object being selected
License requirements: None. |
void |
SelectAMEExtendedObject.setValue(AMEExtendedObject selection,
View view,
Point3d point)
The object being selected with the object's view and object's point
License requirements: None. |
void |
SelectAMEExtendedObject.setValueWithCaeSetObjectInfo(AMEExtendedObject selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObject.setValue(nxopen.TaggedObject) .
|
void |
SelectAMEExtendedObject.setValueWithSnap(InferSnapType.SnapType snapType,
AMEExtendedObject selection1,
View view1,
Point3d point1,
AMEExtendedObject selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.