Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Field and Description |
---|---|
static GeneralAnnotationSettingsBuilder.HorizontalTextPosition |
GeneralAnnotationSettingsBuilder.HorizontalTextPosition.ABOVE |
static GeneralAnnotationSettingsBuilder.HorizontalTextPosition |
GeneralAnnotationSettingsBuilder.HorizontalTextPosition.BELOW |
Modifier and Type | Method and Description |
---|---|
GeneralAnnotationSettingsBuilder.HorizontalTextPosition |
GeneralAnnotationSettingsBuilder.textPositionHorizontal()
Returns the horizontal text position
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
static GeneralAnnotationSettingsBuilder.HorizontalTextPosition |
GeneralAnnotationSettingsBuilder.HorizontalTextPosition.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeneralAnnotationSettingsBuilder.HorizontalTextPosition |
GeneralAnnotationSettingsBuilder.HorizontalTextPosition.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeneralAnnotationSettingsBuilder.HorizontalTextPosition[] |
GeneralAnnotationSettingsBuilder.HorizontalTextPosition.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeneralAnnotationSettingsBuilder.setTextPositionHorizontal(GeneralAnnotationSettingsBuilder.HorizontalTextPosition type)
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.