Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Field and Description |
---|---|
static EngineeringObjectAspectDetailBuilder.NameSource |
EngineeringObjectAspectDetailBuilder.NameSource.DEFAULT |
static EngineeringObjectAspectDetailBuilder.NameSource |
EngineeringObjectAspectDetailBuilder.NameSource.MAPPING |
static EngineeringObjectAspectDetailBuilder.NameSource |
EngineeringObjectAspectDetailBuilder.NameSource.NAMING_RULE |
static EngineeringObjectAspectDetailBuilder.NameSource |
EngineeringObjectAspectDetailBuilder.NameSource.USER_INPUT |
Modifier and Type | Method and Description |
---|---|
static EngineeringObjectAspectDetailBuilder.NameSource |
EngineeringObjectAspectDetailBuilder.NameSource.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EngineeringObjectAspectDetailBuilder.NameSource |
EngineeringObjectAspectDetailBuilder.NameSource.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EngineeringObjectAspectDetailBuilder.NameSource[] |
EngineeringObjectAspectDetailBuilder.NameSource.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EngineeringObjectAspectDetailBuilder.setNameSource(String aspectType,
EngineeringObjectAspectDetailBuilder.NameSource source)
Sets the source for aspect name
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.