public static class EngineeringObjectAspectDetailBuilder.NameSource extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DEFAULT |
static int |
_MAPPING |
static int |
_NAMING_RULE |
static int |
_USER_INPUT |
static EngineeringObjectAspectDetailBuilder.NameSource |
DEFAULT |
static EngineeringObjectAspectDetailBuilder.NameSource |
MAPPING |
static EngineeringObjectAspectDetailBuilder.NameSource |
NAMING_RULE |
static EngineeringObjectAspectDetailBuilder.NameSource |
USER_INPUT |
Modifier and Type | Method and Description |
---|---|
static EngineeringObjectAspectDetailBuilder.NameSource |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EngineeringObjectAspectDetailBuilder.NameSource |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EngineeringObjectAspectDetailBuilder.NameSource[] |
values()
Returns an array that contains the values for this enum.
|
public static final EngineeringObjectAspectDetailBuilder.NameSource DEFAULT
public static final EngineeringObjectAspectDetailBuilder.NameSource NAMING_RULE
public static final EngineeringObjectAspectDetailBuilder.NameSource USER_INPUT
public static final EngineeringObjectAspectDetailBuilder.NameSource MAPPING
public static final int _DEFAULT
public static final int _NAMING_RULE
public static final int _USER_INPUT
public static final int _MAPPING
public static EngineeringObjectAspectDetailBuilder.NameSource valueOf(int value)
public static EngineeringObjectAspectDetailBuilder.NameSource valueOf(String name)
public static EngineeringObjectAspectDetailBuilder.NameSource[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.