Package | Description |
---|---|
nxopen.ame |
Provides classes and interfaces for AME.
|
Modifier and Type | Field and Description |
---|---|
static FormSheetBuilder.SizeOption |
FormSheetBuilder.SizeOption.CUSTOM |
static FormSheetBuilder.SizeOption |
FormSheetBuilder.SizeOption.STANDARD |
Modifier and Type | Method and Description |
---|---|
FormSheetBuilder.SizeOption |
FormSheetBuilder.formSheetSizeOption()
Returns the size option type of type
FormSheetBuilder.SizeOption
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") Created in NX12.0.0 |
static FormSheetBuilder.SizeOption |
FormSheetBuilder.SizeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FormSheetBuilder.SizeOption |
FormSheetBuilder.SizeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FormSheetBuilder.SizeOption[] |
FormSheetBuilder.SizeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FormSheetBuilder.setFormSheetSizeOption(FormSheetBuilder.SizeOption sizeOption)
License requirements: ad_automation_design ("FULL AUTOMATION DESIGNER") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.