AlternateIdManager Class |
This class is responsible for setting and getting NX Manager database attribute. |
AttributeGroup Class |
Represents an attribute group. |
AttributeGroupCollection Class |
Represents a collection of attribute group objects. |
AttributeGroupDescription Class |
Represents an attribute group type. |
AttributeGroupDescriptionCollection Class |
Represents a collection of attribute group description objects. |
AttributeGroupReviseBuilder Class |
Represents an attribute group revise builder. |
CAEFileContainer Class |
This class is a File Container class for uploading JT files created by NX CAE Post Processing to Teamcenter. Users can add the JT file names and their corresponding dataset names to this container class. Once all the JT file names are added, this class can be used to upload the JT files to Teamcenter. The class can be used to upload only to a a single part at a time.
|
CaeCloneManager Class |
This class is used for executing CAE Clone on a Simulation File or a FeModel File.
|
ConditionalElementRevision Class |
Represents a base class that provides common methods for various conditional model elements in a NXOpen.CollaborativeDesign . |
ConfigurationContextBuilder Class |
Represents a NXOpen.PDM.ConfigurationContextBuilder builder |
ConfigurationManager Class |
Represents Configuration Manager |
ConnectionElementRevision Class |
Represents a base class that provides common methods for various model elements in a NXOpen.CollaborativeDesign . |
CrossSheetReference Class |
Represents a base class that provides common methods for various model elements in a NXOpen.CollaborativeDesign . |
CustomWebAppMenuHandler Class |
Represents Custom WebApp Menu Handler class |
DBEntityProxy Class |
JA class for the DBEntityProxy object |
DatabaseAttributeManager Class |
This class is responsible for setting and getting NX Manager database attribute. |
DatabaseObject Class |
Represents a Teamcenter database object |
DatabaseObjectManager Class |
This class is used for retrieving PDM database objects.
|
DatabaseObjects Class |
Represents a collection of NXOpen.PDM.DatabaseObject . |
DesignElementRevision Class |
Represents the design element revision in the database. |
DesignFeatureRevision Class |
Represents the design feature revision in the database. |
DesignSubordinateRevision Class |
Represents the design subordinate revision in the database. |
EffectivityAttributePropertiesBuilder Class |
Represents an NXOpen.PDM.EffectivityAttributePropertiesBuilder to be used for creating effectivity attributes. |
EffectivityTableBuilder Class |
Represents a builder class for effectivity configuration. |
EffectivityTableRow Class |
Represents the class that contains effectivity parameters. |
ElementGroup Class |
Represents a base class that provides common methods for various model elements in a NXOpen.CollaborativeDesign . |
FileManagement Class |
This class is responsible for Teamcenter file management related activities. |
FindCriteria Class |
Represents find criteria objects |
GenericObjectAttributeHolder Class |
Represents the class that contains database business logic or pre-creation information for the objects. |
IAttributeGroupOwner Class |
An interface class for objects that own attribute groups. |
ListOfValues Class |
Represents list of values to be used in search query |
LogicalElementRevision Class |
Represents a base class that provides common methods for various model elements in a NXOpen.CollaborativeDesign . |
LogicalObject Class |
Represents the class that contains database business logic or pre-creation information for the objects. |
ModelElement Class |
Represents a base class that provides common methods for various model elements in a NXOpen.CollaborativeDesign . |
ModelElementRevision Class |
Represents a base class that provides common methods for various model elements in a NXOpen.CollaborativeDesign . |
NativePartLogicalObject Class |
Represents the class that contains information for the objects participating in import operation. |
NonMasterData Class |
Represents a class that performs various operations on NonMaster Datasets |
ObjectCreateBuilder Class |
Represents a builder class that perofrms create operation |
OperationErrors Class |
Represents Operation Errors to be returned in TCIN related operations |
OrderedElementGroup Class |
Represents a base class that provides common methods for ordered elements group in a NXOpen.PDM.ElementGroup . |
PartBuilder Class |
This class serves as the base class for NX Manager part builders. |
PartCreationObject Class |
This class is a proxy for a to-be-created part prior to the part being created. |
PartCreationObjectAttributePropertiesBuilder Class |
Represents an NXOpen.PDM.PartCreationObjectAttributePropertiesBuilder . |
PartFromPartBuilder Class |
This class provides the methods necessary to create a new part in NX Manager from an existing part. |
PartFromTemplateBuilder Class |
This class provides the methods necessary to create a new part in NX Manager from a template part. |
PartManager Class |
This class contains methods to create and manage parts in NX Manager mode. |
PartOperationAttributePropertiesBuilder Class |
Represents an NXOpen.PDM.PartOperationAttributePropertiesBuilder to be used for creating attributes in part operation. |
PartOperationBuilder Class |
Represents a builder class that performs various design element operations. |
PartOperationCopyBuilder Class |
Represents a builder class that performs various Save As operations. |
PartOperationCreateBuilder Class |
Represents a builder class that performs Create operations |
PartOperationImportBuilder Class |
Represents a builder class that performs Create operations |
PartOperationImportCallbackData Class |
JA interface for PartOperationImportCallbackData object |
PartOperationImportObserver Class |
This class is responsible for invoking registered callbacks at different stages in import operation. |
PartOperationMakeUniqueBuilder Class |
Represents a NXOpen.PDM.PartOperationMakeUniqueBuilder builder |
PartOperationValidationPropertiesBuilder Class |
Represents an NXOpen.PDM.PartOperationValidationPropertiesBuilder to be used for overriding the default validation parameters for a part in import operation. |
PdmFile Class |
Contains methods for accessing PDM file data.
|
PdmNavigatorNode Class |
Represents a PdmNavigatorNode |
PdmPart Class |
This class serves as a gateway to part-specific tools for NX Manager mode. |
PdmSearch Class |
Represents search query |
PdmSearchManager Class |
Represents search manager class |
PdmSession Class |
Represents the NX Manager session |
PendingComponentsManager Class |
This class is used for managing a part’s pending components, that is, those that have been added within Teamcenter but are not yet present in NX. |
PersistentSettings Class |
Persistently held settings for a Teamcenter user account. |
PortArtifact Class |
Represents a base class that provides common methods for port artifact in a NXOpen.PDM.LogicalElementRevision . |
RequirementUtils Class |
Collection of PDM utility methods |
SearchResult Class |
Represents search query |
SessionSettings Class |
Values for the settings that affect the current Teamcenter session. |
SheetRevision Class |
Represents a base class that provides common methods for various model elements in a NXOpen.CollaborativeDesign . |
SmartSaveBuilder Class |
TODO: Add a documentation comment describing this class. |
SmartSaveObject Class |
Represents the class for object participating in the smart save operation. |
SoaQuery Class |
Represents search soa query to perform Teamcenter search |
TracelinkQuery Class |
Represents the Trace link query |
VariantConfigurationBuilder Class |
Represents a builder class that performs variant rule configuration. |
WebAppSession Class |
Represents the Web App session |