EffectivityAttributePropertiesBuilder Class¶
-
class
NXOpen.PDM.
EffectivityAttributePropertiesBuilder
¶ Bases:
NXOpen.Builder
Represents an
NXOpen.PDM.EffectivityAttributePropertiesBuilder
to be used for creating effectivity attributes.The attribute will be distributed to all objects supplied in the selected object list.
To create a new instance of this class, use
NXOpen.PDM.ConfigurationManager.CreateEffectivityAttributePropertiesBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Category | Returns or sets the category. |
DisplayValue | Returns or sets the display value. |
EffectivityTableBuilder | Returns the effectivity table builder. |
SelectedObjects | Returns the selected object(s) list. |
StringValue | Returns or sets the string value. |
Tag | Returns the Tag for this object. |
Title | Returns or sets the attribute title. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateAttribute | Create the attribute from the data set in the builder. |
Delete | Delete the attribute from the given object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAttributeObjects | Sets the array of objects that have this attribute |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Category¶
-
EffectivityAttributePropertiesBuilder.
Category
¶ Returns or sets the category.
The category is an optional, user-defined string that allows attributes to be grouped together.
-------------------------------------
Getter Method
Signature
Category()
Returns: Return type: str New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
Category(category)
Parameters: category (str) – New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
DisplayValue¶
-
EffectivityAttributePropertiesBuilder.
DisplayValue
¶ Returns or sets the display value.
Required if creating an attribute of type String.
-------------------------------------
Getter Method
Signature
DisplayValue()
Returns: Return type: str New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
DisplayValue(displayValue)
Parameters: displayValue (str) – New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
EffectivityTableBuilder¶
-
EffectivityAttributePropertiesBuilder.
EffectivityTableBuilder
¶ Returns the effectivity table builder.
-------------------------------------
Getter Method
Signature
EffectivityTableBuilder()
Returns: Return type: NXOpen.PDM.EffectivityTableBuilder
New in version NX9.0.0.
License requirements: None.
SelectedObjects¶
-
EffectivityAttributePropertiesBuilder.
SelectedObjects
¶ Returns the selected object(s) list.
The created attribute will be applied to all objects in this list.
-------------------------------------
Getter Method
Signature
SelectedObjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
StringValue¶
-
EffectivityAttributePropertiesBuilder.
StringValue
¶ Returns or sets the string value.
Required if creating an attribute of type String.
-------------------------------------
Getter Method
Signature
StringValue()
Returns: Return type: str New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
StringValue(stringValue)
Parameters: stringValue (str) – New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Title¶
-
EffectivityAttributePropertiesBuilder.
Title
¶ Returns or sets the attribute title.
The title is required for creating an attribute and must be unique on the given object. Once the attribute is created, the title cannot be modified.
-------------------------------------
Getter Method
Signature
Title()
Returns: Return type: str New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
-------------------------------------
Setter Method
Signature
Title(title)
Parameters: title (str) – New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Method Detail¶
CreateAttribute¶
-
EffectivityAttributePropertiesBuilder.
CreateAttribute
¶ Create the attribute from the data set in the builder.
Unlike calling commit, this method will not perform an update.
Signature
CreateAttribute()
Returns: True if the attribute was created/edited successfully Return type: bool New in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Delete¶
-
EffectivityAttributePropertiesBuilder.
Delete
¶ Delete the attribute from the given object.
Signature
Delete(object)
Parameters: object ( NXOpen.NXObject
) – The object containing the attributeNew in version NX9.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
SetAttributeObjects¶
-
EffectivityAttributePropertiesBuilder.
SetAttributeObjects
¶ Sets the array of objects that have this attribute
Signature
SetAttributeObjects(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsNew in version NX8.5.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
Validate¶
-
EffectivityAttributePropertiesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.