SheetRevision Class¶
-
class
NXOpen.PDM.
SheetRevision
¶ Bases:
NXOpen.PDM.ConditionalElementRevision
Represents a base class that provides common methods for various model elements in a
NXOpen.CollaborativeDesign
.Use the static method in this class to obtain an instance.
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
EffectivityFormula | Returns the formula string that represents the effectivity of this object in database. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningCollaborativeDesign | Returns the owning NXOpen.CollaborativeDesign . |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Create | Creates an attribute group for a NXOpen.PDM.IAttributeGroupOwner , based on an attribute group type. |
CreateAttributeGroupReviseBuilder | Creates a NXOpen.PDM.AttributeGroupReviseBuilder object. |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeGroupDescriptions | Returns the NXOpen.PDM.AttributeGroupDescription objects representing the attribute group types supported by this object. |
GetAttributeGroups | Returns the NXOpen.PDM.AttributeGroup objects owned by this object. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetMemberPartitions | Get all the partitions of this model element revision. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
IsOccurrence¶
-
SheetRevision.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
SheetRevision.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
SheetRevision.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
SheetRevision.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
SheetRevision.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
SheetRevision.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
Create¶
-
SheetRevision.
Create
¶ Creates an attribute group for a
NXOpen.PDM.IAttributeGroupOwner
, based on an attribute group type.An attribute group type is represented by an
NXOpen.PDM.AttributeGroupDescription
.Signature
Create(attributeGroupDescription)
Parameters: attributeGroupDescription ( NXOpen.PDM.AttributeGroupDescription
) –Returns: The new attribute group. Return type: NXOpen.PDM.AttributeGroup
New in version NX9.0.0.
License requirements: None.
CreateAttributeGroupReviseBuilder¶
-
SheetRevision.
CreateAttributeGroupReviseBuilder
¶ Overloaded method CreateAttributeGroupReviseBuilder
CreateAttributeGroupReviseBuilder(attributeGroups)
CreateAttributeGroupReviseBuilder(attributeGroups, keepOriginal, saveAsActionType)
-------------------------------------
Creates a
NXOpen.PDM.AttributeGroupReviseBuilder
object. The builder creates a revision for each attribute group in the input list of existing attribute groups.Signature
CreateAttributeGroupReviseBuilder(attributeGroups)
Parameters: attributeGroups (list of NXOpen.PDM.AttributeGroup
) –Returns: Return type: NXOpen.PDM.AttributeGroupReviseBuilder
New in version NX9.0.0.
License requirements: None.
-------------------------------------
The builder will do a revise or save-as operation for each attribute group in the input list of existing attribute groups depending on input operation type.
Signature
CreateAttributeGroupReviseBuilder(attributeGroups, keepOriginal, saveAsActionType)
Parameters: - attributeGroups (list of
NXOpen.PDM.AttributeGroup
) – - keepOriginal (bool) –
- saveAsActionType (
NXOpen.PDM.AttributeGroupReviseBuilderSaveAsActionType
) –
Returns: Return type: New in version NX11.0.0.
License requirements: None.
-------------------------------------
FindObject¶
-
SheetRevision.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAttributeGroupDescriptions¶
-
SheetRevision.
GetAttributeGroupDescriptions
¶ Returns the
NXOpen.PDM.AttributeGroupDescription
objects representing the attribute group types supported by this object.Signature
GetAttributeGroupDescriptions()
Returns: Return type: list of NXOpen.PDM.AttributeGroupDescription
New in version NX9.0.0.
License requirements: None.
GetAttributeGroups¶
-
SheetRevision.
GetAttributeGroups
¶ Returns the
NXOpen.PDM.AttributeGroup
objects owned by this object.Signature
GetAttributeGroups()
Returns: Return type: list of NXOpen.PDM.AttributeGroup
New in version NX9.0.0.
License requirements: None.
Print¶
-
SheetRevision.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
SheetRevision.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.