PdmPart Class¶
-
class
NXOpen.PDM.
PdmPart
¶ Bases:
object
This class serves as a gateway to part-specific tools for NX Manager mode.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
AssignPermanentName | Assign a permanent name to the temporary part |
CheckinParts | Given an array of parts, check in the parts. |
Checkout | Checkout the part |
CheckoutParts | Given an array of parts, check out the parts. |
NewAlternateIdManager | Create an instance of a NXOpen.PDM.AlternateIdManager class that will be used to create alternate ID information on the part. |
NewDatabaseAttributeManager | Create an instance of a NXOpen.PDM.DatabaseAttributeManager class that will be used to modify database attributes of the part. |
SetDefaultFolderForPart | Set default folder for the part in which it is to be saved |
Structs¶
PdmPartCheckinInput_Struct Struct | Reservation check-in input struct |
PdmPartCheckoutInput_Struct Struct | Reservation check-out input struct |
Method Detail¶
AssignPermanentName¶
-
PdmPart.
AssignPermanentName
¶ Assign a permanent name to the temporary part
Signature
AssignPermanentName(newFileName)
Parameters: newFileName (str) – name of new part file to create New in version NX7.5.0.
License requirements: None.
CheckinParts¶
-
PdmPart.
CheckinParts
¶ Given an array of parts, check in the parts.
Signature
CheckinParts(partsToCheckIn, checkInInput)
Parameters: - partsToCheckIn (list of
NXOpen.BasePart
) – Array of parts to check in - checkInInput (
NXOpen.PDM.PdmPartCheckinInput_Struct
) – Input which control the check in behavior
Returns: Errors encountered during the checkin
Return type: New in version NX8.5.0.
License requirements: None.
- partsToCheckIn (list of
Checkout¶
-
PdmPart.
Checkout
¶ Checkout the part
Signature
Checkout()
New in version NX6.0.0.
License requirements: None.
CheckoutParts¶
-
PdmPart.
CheckoutParts
¶ Given an array of parts, check out the parts.
Signature
CheckoutParts(partsToCheckOut, checkOutInput)
Parameters: - partsToCheckOut (list of
NXOpen.BasePart
) – Array of parts to check out - checkOutInput (
NXOpen.PDM.PdmPartCheckoutInput_Struct
) – Input which control the check out behavior
Returns: Errors encountered during the checkout
Return type: New in version NX8.5.0.
License requirements: None.
- partsToCheckOut (list of
NewAlternateIdManager¶
-
PdmPart.
NewAlternateIdManager
¶ Create an instance of a
NXOpen.PDM.AlternateIdManager
class that will be used to create alternate ID information on the part.Signature
NewAlternateIdManager()
Returns: the new NXOpen.PDM.AlternateIdManager
instanceReturn type: NXOpen.PDM.AlternateIdManager
New in version NX4.0.0.
License requirements: None.
NewDatabaseAttributeManager¶
-
PdmPart.
NewDatabaseAttributeManager
¶ Create an instance of a
NXOpen.PDM.DatabaseAttributeManager
class that will be used to modify database attributes of the part.Signature
NewDatabaseAttributeManager()
Returns: the new NXOpen.PDM.DatabaseAttributeManager
instanceReturn type: NXOpen.PDM.DatabaseAttributeManager
New in version NX5.0.0.
License requirements: None.