AlternateIdManager Class¶
-
class
NXOpen.PDM.
AlternateIdManager
¶ Bases:
NXOpen.TransientObject
This class is responsible for setting and getting NX Manager database attribute.
Use
PDM.PartBuilder.NewAlternateIdManager()
to get the instance of this class.New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
AssignAlternateId | This method generates alternate item and revision IDs and sets these generated values on this manager class. |
AssignAlternateIds | Generates the alternate ID information by calling AssignAlternateIds() . |
AssignAlternateRevId | This method generates an alternate rev ID and sets this generated value on this manager class. |
AssignAlternateRevision | Generates the alternate Revision ID information. |
CreateAlternateIdInformation | Adds the alternate ID information set by calling SetAlternateIdInformation() and the various assign and set methods. |
Dispose | Free resources associated with the instance. |
GetAllContexts | Gets a list of all the available contexts. |
GetAllIdTypes | Gets a list of all the available ID types for a given context. |
GetAlternateDescription | Gets the value of a alternate name as it is currently set on this manager class. |
GetAlternateIdAsDefaultIndentifier | Gets (as it is currently set on this manager class) whether the alternate ID information should be the default indentifier. |
GetAlternateItemId | Gets the value of a alternate ID as it is currently set on this manager class. |
GetAlternateName | Gets the value of a alternate name as it is currently set on this manager class. |
GetAlternateRevId | Gets the value of a alternate rev ID as it is currently set on this manager class. |
GetContext | Gets the value of a context as it is currently set on this manager class. |
GetIdType | Gets the value of a ID type as it is currently set on this manager class. |
SetAlternateDescription | Sets the value of the alternate description. |
SetAlternateIdAsDefaultIndentifier | Sets whether the alternate ID information should be the default indentifier. |
SetAlternateIdInformation | Sets alternate ID information on this manager class. |
SetAlternateItemId | Sets the value of the alternate item ID. |
SetAlternateName | Sets the value of the alternate name. |
SetAlternateRevId | Sets the value of the alternate rev ID. |
SetContext | Sets the value of a context. |
SetIdType | Sets the value of an ID type. |
Structs¶
AlternateIdManagerAlternateIdsData_Struct Struct | Contains alternate Ids data |
AlternateIdManagerAssignAlternateRevData_Struct Struct | Contains alternate Revision Id data |
Method Detail¶
AssignAlternateId¶
-
AlternateIdManager.
AssignAlternateId
¶ This method generates alternate item and revision IDs and sets these generated values on this manager class.
Note that the ID context and type must be set on the builder in order for this assign operation to be successful.
Signature
AssignAlternateId()
Returns: a tuple Return type: A tuple consisting of (alternateItemId, alternateRevId). alternateItemId is a str. the newly generated alternate item ID value that was set on this manager alternateRevId is a str. the newly generated alternate revision ID value that was set on this manager New in version NX4.0.0.
License requirements: None.
AssignAlternateIds¶
-
AlternateIdManager.
AssignAlternateIds
¶ Generates the alternate ID information by calling
AssignAlternateIds()
. Returns pointer to PDM.Altids.AlternateIdsData object. Sets Alternate Name,Alternate Id,Alternate Revision ,Alternate Description, flag for alternate Id modifiable and flag for revision modifiable into Alternate Manager object.Signature
AssignAlternateIds(context, idType)
Parameters: - context (str) – the context
- idType (str) – the Id type
Returns: Contains alternate Ids data
Return type: New in version NX5.0.0.
License requirements: None.
AssignAlternateRevId¶
-
AlternateIdManager.
AssignAlternateRevId
¶ This method generates an alternate rev ID and sets this generated value on this manager class.
Note that the ID context and type must be set on the builder in order for this assign operation to be successful.
Signature
AssignAlternateRevId()
Returns: the newly generated alternate rev ID value that was set on this manager :rtype: str
New in version NX4.0.0.
License requirements: None.
AssignAlternateRevision¶
-
AlternateIdManager.
AssignAlternateRevision
¶ Generates the alternate Revision ID information.
Sets Alternate Revision and flag for revision modifiable into Alternate Manager object.
Signature
AssignAlternateRevision()
Returns: Contains alternate Revision Id data Return type: NXOpen.PDM.AlternateIdManagerAssignAlternateRevData_Struct
New in version NX5.0.0.
License requirements: None.
CreateAlternateIdInformation¶
-
AlternateIdManager.
CreateAlternateIdInformation
¶ Adds the alternate ID information set by calling
SetAlternateIdInformation()
and the various “assign” and “set” methods. The context, ID type, alternate ID, alternate revision ID, and the alternate name must all be set before calling this method.Signature
CreateAlternateIdInformation()
New in version NX4.0.0.
License requirements: None.
Dispose¶
-
AlternateIdManager.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX4.0.0.
License requirements: None.
GetAllContexts¶
-
AlternateIdManager.
GetAllContexts
¶ Gets a list of all the available contexts.
Signature
GetAllContexts()
Returns: list of contexts Return type: list of str New in version NX4.0.0.
License requirements: None.
GetAllIdTypes¶
-
AlternateIdManager.
GetAllIdTypes
¶ Gets a list of all the available ID types for a given context.
Signature
GetAllIdTypes(context)
Parameters: context (str) – the context Returns: list of ID types Return type: list of str New in version NX4.0.0.
License requirements: None.
GetAlternateDescription¶
-
AlternateIdManager.
GetAlternateDescription
¶ Gets the value of a alternate name as it is currently set on this manager class.
Signature
GetAlternateDescription()
Returns: the current value of the alternate description on this manager :rtype: str
New in version NX4.0.0.
License requirements: None.
GetAlternateIdAsDefaultIndentifier¶
-
AlternateIdManager.
GetAlternateIdAsDefaultIndentifier
¶ Gets (as it is currently set on this manager class) whether the alternate ID information should be the default indentifier.
Signature
GetAlternateIdAsDefaultIndentifier()
Returns: the current value of option on this manager :rtype: bool
New in version NX4.0.0.
License requirements: None.
GetAlternateItemId¶
-
AlternateIdManager.
GetAlternateItemId
¶ Gets the value of a alternate ID as it is currently set on this manager class.
Signature
GetAlternateItemId()
Returns: the current value of the alternate item ID on this manager Return type: str New in version NX4.0.0.
License requirements: None.
GetAlternateName¶
-
AlternateIdManager.
GetAlternateName
¶ Gets the value of a alternate name as it is currently set on this manager class.
Signature
GetAlternateName()
Returns: the current value of the alternate name on this manager :rtype: str
New in version NX4.0.0.
License requirements: None.
GetAlternateRevId¶
-
AlternateIdManager.
GetAlternateRevId
¶ Gets the value of a alternate rev ID as it is currently set on this manager class.
Signature
GetAlternateRevId()
Returns: the current value of the alternate rev ID on this manager :rtype: str
New in version NX4.0.0.
License requirements: None.
GetContext¶
-
AlternateIdManager.
GetContext
¶ Gets the value of a context as it is currently set on this manager class.
Signature
GetContext()
Returns: the current value of the context on this manager Return type: str New in version NX4.0.0.
License requirements: None.
GetIdType¶
-
AlternateIdManager.
GetIdType
¶ Gets the value of a ID type as it is currently set on this manager class.
Signature
GetIdType()
Returns: the current value of the ID type on this manager Return type: str New in version NX4.0.0.
License requirements: None.
SetAlternateDescription¶
-
AlternateIdManager.
SetAlternateDescription
¶ Sets the value of the alternate description.
Signature
SetAlternateDescription(alternateDescription)
Parameters: alternateDescription (str) – the new value the alternate description is to be set to New in version NX4.0.0.
License requirements: None.
SetAlternateIdAsDefaultIndentifier¶
-
AlternateIdManager.
SetAlternateIdAsDefaultIndentifier
¶ Sets whether the alternate ID information should be the default indentifier.
Signature
SetAlternateIdAsDefaultIndentifier(alternateIdAsDefaultIndentifier)
Parameters: alternateIdAsDefaultIndentifier (bool) – the new value the option is to be set to New in version NX4.0.0.
License requirements: None.
SetAlternateIdInformation¶
-
AlternateIdManager.
SetAlternateIdInformation
¶ Sets alternate ID information on this manager class.
None can be specified for parameters which are set via other set or assign methods on this builder.
Signature
SetAlternateIdInformation(context, idType, alternateItemId, alternateRevId, alternateName, alternateDescription, alternateIdAsDefaultIndentifier)
Parameters: - context (str) – the new value the context is to be set to
- idType (str) – the new value the ID type is to be set to
- alternateItemId (str) – the new value the alternate item ID is to be set to
- alternateRevId (str) – the new value the alternate rev ID is to be set to
- alternateName (str) – the new value the alternate name is to be set to
- alternateDescription (str) – the new value the alternate description is to be set to
- alternateIdAsDefaultIndentifier (bool) – the new value the option is to be set to
New in version NX4.0.0.
License requirements: None.
SetAlternateItemId¶
-
AlternateIdManager.
SetAlternateItemId
¶ Sets the value of the alternate item ID.
Signature
SetAlternateItemId(alternateItemId)
Parameters: alternateItemId (str) – the new value the alternate item ID is to be set to New in version NX4.0.0.
License requirements: None.
SetAlternateName¶
-
AlternateIdManager.
SetAlternateName
¶ Sets the value of the alternate name.
Signature
SetAlternateName(alternateName)
Parameters: alternateName (str) – the new value the alternate name is to be set to New in version NX4.0.0.
License requirements: None.
SetAlternateRevId¶
-
AlternateIdManager.
SetAlternateRevId
¶ Sets the value of the alternate rev ID.
Signature
SetAlternateRevId(alternateRevId)
Parameters: alternateRevId (str) – the new value the alternate rev ID is to be set to New in version NX4.0.0.
License requirements: None.