PartOperationImportBuilderExistingPartAction Enumeration¶
NXOpen.PDM.PartOperationImportBuilder.ExistingPartAction is an alias for NXOpen.PDM.PartOperationImportBuilderExistingPartAction
-
class
NXOpen.PDM.
PartOperationImportBuilderExistingPartAction
¶ Bases:
object
This enum is used to specify the default action for import.
Enum Members
Enum Member Enum Member Description Overwrite UseExisting NewRevision Default -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-