SmartSaveBuilderSaveType Enumeration¶
NXOpen.PDM.SmartSaveBuilder.SaveType is an alias for NXOpen.PDM.SmartSaveBuilderSaveType
-
class
NXOpen.PDM.
SmartSaveBuilderSaveType
¶ Bases:
object
Represents an File Save type
New in version NX11.0.0.
Enum Members
Enum Member Enum Member Description Save File SaveSaveAll File SaveAllSavePreciseAssembly File SavePreciseAssemblySaveWorkPartOnly File SaveWorkPartOnlySaveAndClose File Save And Close-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-