SmartSaveBuilder Class¶
-
class
NXOpen.PDM.
SmartSaveBuilder
¶ Bases:
NXOpen.Builder
,NXOpen.IAttributeSourceObjectBuilder
TODO: Add a documentation comment describing this class.
The comment must be placed inside and should describe conceptually what this class represents or does. Don’t use a comment that just states something that would be obvious if the comment didn’t exist. Such comments add no value for the customer. To create a new instance of this class, use
NXOpen.PDM.PdmSession.CreateSmartSaveBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DebugDumpEnabled | Returns or sets the debug dump enabled |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AutoAssignAttributes | Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign. |
CanPerformDefaultSave | Checks whether smart save operation can be performed with default operation type set @return |
ClearValidationFailures | Clears operation failures if any |
Commit | Commits any edits that have been applied to the builder. |
CreateSpecificationsForSmartSaveObjects | Create new specifications for Logical Objects |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOperationFailures | Returns operation failures @return |
GetSmartSaveObjects | Gets the smart save objects for the modified objects in session. |
OnOperationTypeChanged | Updates the given smart save objects after operation type change. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateSmartSaveObjectsOnBuilder | Updates the smart save objects with valid operation type and dependencies |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateSmartSaveObjects | Validates whether the save operation can be performed on the smart save objects |
Enumerations¶
SmartSaveBuilderSaveType Enumeration | Represents an File Save type |
Property Detail¶
DebugDumpEnabled¶
-
SmartSaveBuilder.
DebugDumpEnabled
¶ Returns or sets the debug dump enabled
-------------------------------------
Getter Method
Signature
DebugDumpEnabled()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DebugDumpEnabled(debugDumpEnabled)
Parameters: debugDumpEnabled (bool) – New in version NX11.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
Method Detail¶
AutoAssignAttributes¶
-
SmartSaveBuilder.
AutoAssignAttributes
¶ Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
Signature
AutoAssignAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) –Returns: Return type: NXOpen.ErrorList
New in version NX8.5.0.
License requirements: None.
CanPerformDefaultSave¶
-
SmartSaveBuilder.
CanPerformDefaultSave
¶ Checks whether smart save operation can be performed with default operation type set
Signature
CanPerformDefaultSave()
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
ClearValidationFailures¶
-
SmartSaveBuilder.
ClearValidationFailures
¶ Clears operation failures if any
Signature
ClearValidationFailures()
New in version NX11.0.0.
License requirements: None.
CreateSpecificationsForSmartSaveObjects¶
-
SmartSaveBuilder.
CreateSpecificationsForSmartSaveObjects
¶ Create new specifications for Logical Objects
Signature
CreateSpecificationsForSmartSaveObjects(smartSaveObjects)
Parameters: smartSaveObjects (list of NXOpen.PDM.SmartSaveObject
) –New in version NX11.0.0.
License requirements: None.
GetOperationFailures¶
-
SmartSaveBuilder.
GetOperationFailures
¶ Returns operation failures
Signature
GetOperationFailures()
Returns: Return type: NXOpen.ErrorList
New in version NX11.0.0.
License requirements: None.
GetSmartSaveObjects¶
-
SmartSaveBuilder.
GetSmartSaveObjects
¶ Gets the smart save objects for the modified objects in session.
Signature
GetSmartSaveObjects()
Returns: Return type: list of NXOpen.PDM.SmartSaveObject
New in version NX11.0.0.
License requirements: None.
OnOperationTypeChanged¶
-
SmartSaveBuilder.
OnOperationTypeChanged
¶ Updates the given smart save objects after operation type change.
Signature
OnOperationTypeChanged(smartSaveObjects, operationType)
Parameters: - smartSaveObjects (list of
NXOpen.PDM.SmartSaveObject
) – the objects for which operation type is changed - operationType (
NXOpen.AttributePropertiesBuilderOperationType
) – the new operation type
New in version NX11.0.0.
License requirements: None.
- smartSaveObjects (list of
UpdateSmartSaveObjectsOnBuilder¶
-
SmartSaveBuilder.
UpdateSmartSaveObjectsOnBuilder
¶ Updates the smart save objects with valid operation type and dependencies
Signature
UpdateSmartSaveObjectsOnBuilder()
New in version NX11.0.0.
License requirements: None.
Validate¶
-
SmartSaveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.