PdmSession Class¶
-
class
NXOpen.PDM.
PdmSession
¶ Bases:
object
Represents the NX Manager session
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX7.5.0.
- “AttributeGroupDescriptions”, ” Returns a collection of <ja_class>NXOpen.PDM.AttributeGroupDescription</ja_class> objects representing
- attribute group types. The collection contains attribute group descriptions for <ja_class>NXOpen.PDM.IAttributeGroupOwner</ja_class> objects loaded within the NX session. Use the <ja_method>NXOpen.PDM.IAttributeGroupOwner.GetAttributeGroupDescriptions</ja_method> to get the specific attribute group descriptions for an attribute group owner. “
“PartOperationImportObserver”, ” Returns the <ja_class>NXOpen.PDM.PartOperationImportObserver</ja_class> belonging to this session “
Methods¶
AttributeGroupDescriptions¶
-
PdmSession.
AttributeGroupDescriptions
¶ Returns a collection of
NXOpen.PDM.AttributeGroupDescription
objects representing attribute group types.The collection contains attribute group descriptions for
NXOpen.PDM.IAttributeGroupOwner
objects loaded within the NX session. Use theNXOpen.PDM.IAttributeGroupOwner.GetAttributeGroupDescriptions()
to get the specific attribute group descriptions for an attribute group owner.Signature
AttributeGroupDescriptions()
New in version NX9.0.0.
Returns: Return type: NXOpen.PDM.AttributeGroupDescriptionCollection
PartOperationImportObserver¶
-
PdmSession.
PartOperationImportObserver
¶ Returns the
NXOpen.PDM.PartOperationImportObserver
belonging to this sessionSignature
PartOperationImportObserver()
New in version NX10.0.0.
Returns: Return type: NXOpen.PDM.PartOperationImportObserver
Method Detail¶
CreateCopyOperationBuilder¶
-
PdmSession.
CreateCopyOperationBuilder
¶ Returns a new
NXOpen.PDM.PartOperationCopyBuilder
objectSignature
CreateCopyOperationBuilder(operation)
Parameters: operation ( NXOpen.PDM.PartOperationBuilderOperationType
) –Returns: Return type: NXOpen.PDM.PartOperationCopyBuilder
New in version NX10.0.0.
License requirements: None.
CreateCreateOperationBuilder¶
-
PdmSession.
CreateCreateOperationBuilder
¶ Returns a new
NXOpen.PDM.PartOperationCreateBuilder
objectSignature
CreateCreateOperationBuilder(operation)
Parameters: operation ( NXOpen.PDM.PartOperationBuilderOperationType
) –Returns: Return type: NXOpen.PDM.PartOperationCreateBuilder
New in version NX10.0.0.
License requirements: None.
CreateImportOperationBuilder¶
-
PdmSession.
CreateImportOperationBuilder
¶ Returns a new
NXOpen.PDM.PartOperationImportBuilder
objectSignature
CreateImportOperationBuilder()
Returns: Return type: NXOpen.PDM.PartOperationImportBuilder
New in version NX10.0.0.
License requirements: None.
CreateMakeUniqueOperationBuilder¶
-
PdmSession.
CreateMakeUniqueOperationBuilder
¶ Returns a new
NXOpen.PDM.PartOperationMakeUniqueBuilder
objectSignature
CreateMakeUniqueOperationBuilder(part)
Parameters: part ( NXOpen.BasePart
) –Returns: Return type: NXOpen.PDM.PartOperationMakeUniqueBuilder
New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
CreateObjectCreateBuilder¶
-
PdmSession.
CreateObjectCreateBuilder
¶ Returns a new
NXOpen.PDM.ObjectCreateBuilder
objectSignature
CreateObjectCreateBuilder(tcTypes, baseTCTypes)
Parameters: - tcTypes (list of str) –
- baseTCTypes (list of str) –
Returns: Return type: New in version NX10.0.0.
License requirements: None.
CreateOperationBuilder¶
-
PdmSession.
CreateOperationBuilder
¶ Returns a new
NXOpen.PDM.PartOperationBuilder
objectSignature
CreateOperationBuilder(operation)
Parameters: operation ( NXOpen.PDM.PartOperationBuilderOperationType
) –Returns: Return type: NXOpen.PDM.PartOperationBuilder
New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PdmSession.CreateCopyOperationBuilder()
insteadLicense requirements: None.
CreatePartOperationAttributePropertiesBuilder¶
-
PdmSession.
CreatePartOperationAttributePropertiesBuilder
¶ Creates a new
NXOpen.PDM.PartOperationAttributePropertiesBuilder
object.Signature
CreatePartOperationAttributePropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.PDM.PartOperationAttributePropertiesBuilder
New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
CreatePartOperationValidationPropertiesBuilder¶
-
PdmSession.
CreatePartOperationValidationPropertiesBuilder
¶ Creates a new
AttributePropertiesBuilder
object.Signature
CreatePartOperationValidationPropertiesBuilder(objects)
Parameters: objects (list of NXOpen.NXObject
) – the array of objectsReturns: Return type: NXOpen.AttributePropertiesBuilder
New in version NX10.0.0.
License requirements: assemblies (“ASSEMBLIES MODULE”)
CreateSmartSaveBuilder¶
-
PdmSession.
CreateSmartSaveBuilder
¶ Creates a new
SmartSaveBuilder
object.Signature
CreateSmartSaveBuilder(saveType)
Parameters: saveType ( NXOpen.PDM.SmartSaveBuilderSaveType
) –Returns: Return type: NXOpen.PDM.SmartSaveBuilder
New in version NX11.0.0.
License requirements: None.
GetDatabaseObjectManager¶
-
PdmSession.
GetDatabaseObjectManager
¶ Gets the
NXOpen.PDM.DatabaseObjectManager
object.Signature
GetDatabaseObjectManager()
Returns: Return type: NXOpen.PDM.DatabaseObjectManager
New in version NX11.0.0.
License requirements: None.
GetSsoSettings¶
-
PdmSession.
GetSsoSettings
¶ Returns the SSO credentials, if SSO is available The client applications can use these settings to connect to the same Tcserver that NX is using.
Signature
GetSsoSettings()
Returns: a tuple Return type: A tuple consisting of (isSsoEnabled, ssoServerUrl, ssoAppID). isSsoEnabled is a bool. if SSO is enabled ssoServerUrl is a str. the SSO server URL ssoAppID is a str. the SSO app id New in version NX10.0.0.
License requirements: None.
GetTcserverSettings¶
-
PdmSession.
GetTcserverSettings
¶ Returns the connect string and discriminator used by NX session to connect to the Tcserver.
The client applications can use these settings to connect to the same Tcserver that NX is using.
Tcserver connect string: The connect string is path of the server hosting the services. The connect string for the different transport protocols will be in the following form: 4-Tier(HTTP mode): similar to http: 2-Tier(IIOP mode): The Tcserver IOR string
Discriminator: The discriminator is a unique identifier and contains unique information related to a given TC server. This unique identifier (discriminator) is recognized by TC pool manager as the session number that ties the server process to the client. The discriminator functionality is part of the SOA package. The discriminator allows multiple clients to connect to the same TC server. In 2-Tier(IIOP mode), the discriminator will be an empty string.
To connect to the same Tcserver as NX, the client can create a Teamcenter::Soa::Client::Connection object using the connect string and then use the Teamcenter::Services::Core::SessionService to login to Teamcenter Server with the discriminator and the connection object. More information about connecting to the Teamcenter server can be found in the TC SOA API Documentation.
Signature
GetTcserverSettings()
Returns: a tuple Return type: A tuple consisting of (connectString, discriminator). connectString is a str. the connection string discriminator is a str. the discriminator New in version NX7.5.0.
License requirements: None.
NewCaeFileContainer¶
-
PdmSession.
NewCaeFileContainer
¶ Returns a new
NXOpen.PDM.CAEFileContainer
objectSignature
NewCaeFileContainer()
Returns: Return type: NXOpen.PDM.CAEFileContainer
New in version NX8.5.0.
License requirements: None.
NewFileManagement¶
-
PdmSession.
NewFileManagement
¶ Returns a new
NXOpen.PDM.FileManagement
objectSignature
NewFileManagement()
Returns: Return type: NXOpen.PDM.FileManagement
New in version NX7.5.4.
License requirements: None.
SetDefaultFolder¶
-
PdmSession.
SetDefaultFolder
¶ Sets default folder.
The input default folder path in format <username>:<folder>:<folder>, where username is optional. In that case, in :<folder>:<folder>, the first : indicates Home, for example, :Newstuff, is the Newstuff folder in current user’s Home container
Signature
SetDefaultFolder(defaultFolderSpec)
Parameters: defaultFolderSpec (str) – Default folder path including default folder name to be set New in version NX7.5.0.
License requirements: None.