PartOperationCreateBuilder Class¶
-
class
NXOpen.PDM.
PartOperationCreateBuilder
¶ Bases:
NXOpen.PDM.PartOperationBuilder
Represents a builder class that performs Create operations
To create a new instance of this class, use
NXOpen.PDM.PdmSession.CreateCreateOperationBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
DefaultDestinationFolder | Returns or sets the default destination folder string for the part being created . |
DependentFileSaveAsOption | Returns or sets the Dependent files Save As option. |
ReplaceAllComponents | Returns or sets the replace all components. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddRelatedPartToOperate | Add related part to the part undergoing an operation. |
AutoAssignAttributes | Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign. |
Commit | Commits any edits that have been applied to the builder. |
CreateLogicalObjects | Creates the pre-creation objects for the parts |
CreateNonMasterListForLogicalObject | Create NonMaster list for the selected logical Object |
CreateSpecificationsForLogicalObjects | Create new specifications for Logical Objects |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditNonMasterName | Sets the name the non-master part will get saved as. |
GetAddMaster | Returns logical value to indicate whether master to be added as child component @return whether master to be added as child component |
GetAlternateIDManager | Create an instance of a NXOpen.PDM.AlternateIdManager class that will be used to create alternate ID information while creating the new part. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDialogOperation | Returns the dialog operation Applicable only for operation types PartOperationBuilderOperationType.SaveAs and PartOperationBuilderOperationType.Revise @return |
GetNonMasterCopyOption | Get the nonmasters saveAs option for given logical object. |
GetNonMasterList | Gets NonMaster list for the given logical Object @return Non-master part file names |
GetObject | Returns the object currently being edited by this builder. |
GetOperationFailures | Returns part operation failures @return |
GetOperationSubType | Returns the NXOpen.PDM.PartOperationCreateBuilderOperationSubType for Create. |
IsNonMasterBeingCopied | Returns whether or not the non master part specified for the given :py:class:`NXOpen.PDM.LogicalObject`will actually get saved during the save as operation. |
SetAddMaster | Sets the Add Master Flag Use this only in case creating a new Altrep. |
SetDialogOperation | Sets the dialog operation. |
SetItemType | Sets the selected Item Type |
SetMasterPart | Sets the Master Part Use this only in case the part your are trying to create supports master model. |
SetModelType | Sets the selected Model Type This is same as the Relation Type that is set by NXOpen.FileNew.RelationType() and is same as the relation type specified in Template PAX files. |
SetNonMasterSaveAsOption | Set the nonmasters saveAs option for given logical object |
SetOperationSubType | Sets the NXOpen.PDM.PartOperationCreateBuilderOperationSubType for Create. |
SetPartSpecToOpen | Sets the Part Spec of the part to open in case of Select Template Dialog This is only applicable if NXOpen.PDM.PartOperationCreateBuilderOperationSubType is set to NXOpen.PDM.PartOperationCreateBuilderOperationSubType.SelectTemplate partSpecTopOpen can be a CLI format (<@>DB/MFKID/RevId) or full TCIN file specification (starting with %UGMGR) |
SetPartsToRename | Sets the Parts To Rename on the Builder. |
SetSelectedNonMasterToSaveAs | Sets whether or not the non-master part specified will actually get saved during the save as operation. |
SetSelectedParts | Sets the selected parts. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateLogicalObjectsToCommit | Validates NXOpen.PDM.LogicalObject objects with this builder and udpates the operation failuers. |
Enumerations¶
PartOperationCreateBuilderOperationSubType Enumeration | Represents an operation sub type for creating a part |
Method Detail¶
AutoAssignAttributes¶
-
PartOperationCreateBuilder.
AutoAssignAttributes
¶ Auto assigns the attributes for a given array of objects and returns an array of objects that failed to auto assign.
Signature
AutoAssignAttributes(objects)
Parameters: objects (list of NXOpen.NXObject
) –Returns: Return type: NXOpen.ErrorList
New in version NX8.5.0.
License requirements: None.
GetAddMaster¶
-
PartOperationCreateBuilder.
GetAddMaster
¶ Returns logical value to indicate whether master to be added as child component
Signature
GetAddMaster()
Returns: whether master to be added as child component Return type: bool New in version NX10.0.0.
License requirements: None.
GetOperationSubType¶
-
PartOperationCreateBuilder.
GetOperationSubType
¶ Returns the
NXOpen.PDM.PartOperationCreateBuilderOperationSubType
for Create.Signature
GetOperationSubType()
Returns: Return type: NXOpen.PDM.PartOperationCreateBuilderOperationSubType
New in version NX10.0.0.
License requirements: None.
SetAddMaster¶
-
PartOperationCreateBuilder.
SetAddMaster
¶ Sets the Add Master Flag Use this only in case creating a new Altrep.
This will add master as a component to newly created master. This will be set to false if tempalte selected doesn’t supports creating new altrep.
Signature
SetAddMaster(addMaster)
Parameters: addMaster (bool) – New in version NX10.0.0.
License requirements: None.
SetItemType¶
-
PartOperationCreateBuilder.
SetItemType
¶ Sets the selected Item Type
Signature
SetItemType(itemType)
Parameters: itemType (str) – New in version NX10.0.0.
License requirements: None.
SetMasterPart¶
-
PartOperationCreateBuilder.
SetMasterPart
¶ Sets the Master Part Use this only in case the part your are trying to create supports master model.
Signature
SetMasterPart(masterPart)
Parameters: masterPart ( NXOpen.BasePart
) –New in version NX10.0.0.
License requirements: None.
SetModelType¶
-
PartOperationCreateBuilder.
SetModelType
¶ Sets the selected Model Type This is same as the Relation Type that is set by
NXOpen.FileNew.RelationType()
and is same as the relation type specified in Template PAX files.This is needed to be set only when the
NXOpen.PDM.PartOperationCreateBuilderOperationSubType
is set toNXOpen.PDM.PartOperationCreateBuilderOperationSubType.CreateSpecification
. In other cases this is read from the Template. If not set this is always assumed to be “master”. Example strings are “specification”, “manifestation”, etc.Signature
SetModelType(modelType)
Parameters: modelType (str) – New in version NX10.0.0.
License requirements: None.
SetOperationSubType¶
-
PartOperationCreateBuilder.
SetOperationSubType
¶ Sets the
NXOpen.PDM.PartOperationCreateBuilderOperationSubType
for Create.Signature
SetOperationSubType(operatioSubType)
Parameters: operatioSubType ( NXOpen.PDM.PartOperationCreateBuilderOperationSubType
) –New in version NX10.0.0.
License requirements: None.
SetPartSpecToOpen¶
-
PartOperationCreateBuilder.
SetPartSpecToOpen
¶ Sets the Part Spec of the part to open in case of Select Template Dialog This is only applicable if
NXOpen.PDM.PartOperationCreateBuilderOperationSubType
is set toNXOpen.PDM.PartOperationCreateBuilderOperationSubType.SelectTemplate
partSpecTopOpen can be a CLI format (<@>DB/MFKID/RevId) or full TCIN file specification (starting with %UGMGR)Signature
SetPartSpecToOpen(partSpecToOpen)
Parameters: partSpecToOpen (str) – New in version NX10.0.0.
License requirements: None.
SetPartsToRename¶
-
PartOperationCreateBuilder.
SetPartsToRename
¶ Sets the Parts To Rename on the Builder.
This is only applicable if
NXOpen.PDM.PartOperationCreateBuilderOperationSubType
is set toNXOpen.PDM.PartOperationCreateBuilderOperationSubType.Rename
Signature
SetPartsToRename(partsToRename)
Parameters: partsToRename (list of NXOpen.BasePart
) –New in version NX10.0.0.
License requirements: None.
Validate¶
-
PartOperationCreateBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.