PartOperationBuilderDependentFileSaveAs Enumeration¶
NXOpen.PDM.PartOperationBuilder.DependentFileSaveAs is an alias for NXOpen.PDM.PartOperationBuilderDependentFileSaveAs
-
class
NXOpen.PDM.
PartOperationBuilderDependentFileSaveAs
¶ Bases:
object
This enum is used to specify which dependent files should be saved during the save as operation.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCopyBuilderCopyDependentFiles
insteadEnum Members
Enum Member Enum Member Description All save all during save asNotSet save none during save as-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-