CaeCloneManager Class¶
-
class
NXOpen.PDM.
CaeCloneManager
¶ Bases:
NXOpen.TransientObject
This class is used for executing CAE Clone on a Simulation File or a FeModel File.
Use
NXOpen.PDM.PartManager
to get the instance of this class.New in version NX9.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCopyBuilder
instead.
Methods¶
Method | Description |
---|---|
CommitClone | Commits the Clone Operation for the Clone Manager class NXOpen.PDM.CaeCloneManager . |
Dispose | Free resources associated with the instance. |
GetContainer | Gets the container in Teamcenter where the cloned part is saved @return |
GetPartBuilderForClone | Get Part Builders for Clone Operation of a CAE Simulation or a CAE Model part. |
SetContainer | Sets the container in Teamcenter where the cloned part is saved |
SetIncludeMaster | Sets the option for include master on the Clone Manager class |
Enumerations¶
CaeCloneManagerCloneOption Enumeration | Option for creation of part builder for CAE Clone |
Method Detail¶
CommitClone¶
-
CaeCloneManager.
CommitClone
¶ Commits the Clone Operation for the Clone Manager class
NXOpen.PDM.CaeCloneManager
.Deletes all the Part Builders associated with the Clone Manager
Signature
CommitClone()
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Dispose¶
-
CaeCloneManager.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX9.0.0.
License requirements: None.
GetContainer¶
-
CaeCloneManager.
GetContainer
¶ Gets the container in Teamcenter where the cloned part is saved
Signature
GetContainer(option)
Parameters: option ( NXOpen.PDM.CaeCloneManagerCloneOption
) –Returns: Return type: str New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetPartBuilderForClone¶
-
CaeCloneManager.
GetPartBuilderForClone
¶ Get Part Builders for Clone Operation of a CAE Simulation or a CAE Model part.
Get builder class
NXOpen.PDM.PartFromPartBuilder
using this function.Signature
GetPartBuilderForClone(option)
Parameters: option ( NXOpen.PDM.CaeCloneManagerCloneOption
) –Returns: the part builder Return type: NXOpen.PDM.PartFromPartBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetContainer¶
-
CaeCloneManager.
SetContainer
¶ Sets the container in Teamcenter where the cloned part is saved
Signature
SetContainer(option, container)
Parameters: - option (
NXOpen.PDM.CaeCloneManagerCloneOption
) – - container (str) –
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- option (
SetIncludeMaster¶
-
CaeCloneManager.
SetIncludeMaster
¶ Sets the option for include master on the Clone Manager class
Signature
SetIncludeMaster(value)
Parameters: value (bool) – New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)