RequirementUtils Class¶
-
class
NXOpen.PDM.
RequirementUtils
¶ Bases:
object
Collection of PDM utility methods
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX6.0.3.
Methods¶
Method | Description |
---|---|
CreateTraceLinks | Creates Trace Links from :py:class:`NXOpen.Validate.Requirement`s to :py:class:`NXOpen.Part`s For the input requirement_item_numbers: In case of Default Domain: it is Teamcenter item ID. |
NewTracelinkQuery | Returns a Tracelink query object @return |
RemoveTraceLinks | Removes Trace Links between :py:class:`NXOpen.Validate.Requirement`s and :py:class:`NXOpen.Part`s For the input requirement_item_numbers: In case of Default Domain: it is Teamcenter item ID. |
Method Detail¶
CreateTraceLinks¶
-
RequirementUtils.
CreateTraceLinks
¶ Creates Trace Links from :py:class:`NXOpen.Validate.Requirement`s to :py:class:`NXOpen.Part`s For the input requirement_item_numbers: In case of Default Domain: it is Teamcenter item ID.
In case of non-Default Domain: it is the multifield key. e.g. %#MFK#%,=item_id=001, object_type=SupplierPart, supplier_code=x And the encoded part filename would be containing the MFK.
Signature
CreateTraceLinks(requirementItemNumbers, requirementRevisions, parts)
Parameters: - requirementItemNumbers (list of str) – requirement multifield key
- requirementRevisions (list of str) – requirement item revisions. Must be same size as the item number array
- parts (list of str) – part CLI names
New in version NX8.5.0.
License requirements: None.
NewTracelinkQuery¶
-
RequirementUtils.
NewTracelinkQuery
¶ Returns a Tracelink query object
Signature
NewTracelinkQuery()
Returns: Return type: NXOpen.PDM.TracelinkQuery
New in version NX6.0.3.
License requirements: None.
RemoveTraceLinks¶
-
RequirementUtils.
RemoveTraceLinks
¶ Removes Trace Links between :py:class:`NXOpen.Validate.Requirement`s and :py:class:`NXOpen.Part`s For the input requirement_item_numbers: In case of Default Domain: it is Teamcenter item ID.
In case of non-Default Domain: it is the multifield key. e.g. %#MFK#%,=item_id=001, object_type=SupplierPart, supplier_code=x And the encoded part filename would be containing the MFK.
Signature
RemoveTraceLinks(requirementItemNumbers, requirementRevisions, parts)
Parameters: - requirementItemNumbers (list of str) – requirement multifield Key
- requirementRevisions (list of str) – requirement item revisions. Must be same size as the item number array
- parts (list of str) – part CLI names
New in version NX8.5.0.
License requirements: None.