PartOperationImportBuilderConversionRule Enumeration¶
NXOpen.PDM.PartOperationImportBuilder.ConversionRule is an alias for NXOpen.PDM.PartOperationImportBuilderConversionRule
-
class
NXOpen.PDM.
PartOperationImportBuilderConversionRule
¶ Bases:
object
This enum is used to specify the conversion rule for
NXOpen.PDM.PartOperationImportBuilderNumberingSourceOption.OSFilename
.Enum Members
Enum Member Enum Member Description AsID AsIDandRevision WithPrefix WithSuffix WithReplaceString -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-