PartFromPartBuilderFileSaveAs Enumeration¶
NXOpen.PDM.PartFromPartBuilder.FileSaveAs is an alias for NXOpen.PDM.PartFromPartBuilderFileSaveAs
-
class
NXOpen.PDM.
PartFromPartBuilderFileSaveAs
¶ Bases:
object
This enum is used to specify which non-master parts and dependent files should be saved during the save as operation.
Enum Members
Enum Member Enum Member Description Some save selected during save asAll save all during save asNotSet save none during save as-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-