PartBuilderOperation Enumeration¶
NXOpen.PDM.PartBuilder.Operation is an alias for NXOpen.PDM.PartBuilderOperation
-
class
NXOpen.PDM.
PartBuilderOperation
¶ Bases:
object
Tokens identifying every possible UG/Manager part selection dialog.
Enum Members
Enum Member Enum Member Description ExportPartNew File-<ja_gt>Export-<ja_gt>NXOpen.Part:New radio buttonAssemblyDiagram Assembly-<ja_gt>Report-<ja_gt>Assembly Diagram...AssemblyCreateNewComponent Assembly-<ja_gt>NXOpen.Assemblies.Component-<ja_gt>Create New...Default Default UG/Manager part selection dialog-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-