AutotestPrint Class |
Represents a class that is used for LineDesigner testing. |
ColumnFeature Class |
Represents a column feature feature |
ColumnFeatureBuilder Class |
Represents a LineDesigner.ColumnFeature Features. |
ColumnGridEquipmentBuilder Class |
Represents a LineDesigner. |
ConnectionCreatorBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreateConnectionCreatorBuilder`</para>Default values. |
ConveyorStationFeature Class |
Represents a conveyor station feature feature |
ConveyorStationFeatureBuilder Class |
Represents a LineDesigner.ConveyorStationFeature builder |
CoverFeature Class |
Represents a cover feature |
CoverFeatureBuilder Class |
Represents a LineDesigner.CoverFeature builder |
CreateFactoryElement Class |
Represents a create factory element |
CreateFactoryElementBuilder Class |
Represents a LineDesigner.CreateFactoryElement builder |
CreateFence Class |
Represents a create fence |
CreateFenceBuilder Class |
Represents a LineDesigner.CreateFence builder |
CreateSystem Class |
Represents a create system |
CreateSystemBuilder Class |
Represents a LineDesigner.CreateSystem builder |
DBColumnGridNode Class |
Represents DB column grid node |
DBConveyorNode Class |
Represents DB conveyor node |
DBFactoryCadGeoNode Class |
Represents DB import factory cad geo node |
DBFactoryNode Class |
Represents DB factory node |
DBFenceNode Class |
Represents DB factory node |
DBFloorEquipmentNode Class |
Represents DB Floor equipment node |
DBNode Class |
Represents DB node |
DBNodeContainer Class |
Represents DB node container |
DBNodeManager Class |
Represents a manager of line designer db nodes |
DBNodeUtils Class |
Represents a utils of line designer for journaling uinode methods |
DBPlatformEquipmentNode Class |
Represents DB platform equipment node |
DBSmartComplexEquipmentNode Class |
Represents DB factory node |
DBSmartEquipmentNode Class |
Represents DB factory node |
DBStairwayEquipmentNode Class |
Represents DB stairway equipment node |
DiamondConnectorFeature Class |
Represents a typed connector feature feature |
DisconnectConnectionBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreateDisconnectConnectionBuilder`</para> |
ExportPlantToDWG Class |
Represents the export plant to dwg |
ExportPlantToDWGBuilder Class |
Represents a LineDesigner.ExportPlantToDWG builder |
ExportToDWG Class |
Represents an export to dwg |
ExportToDWGBuilder Class |
Represents a LineDesigner.ExportToDWG builder |
FastPlacementUtilityBuilder Class |
Fast Placement |
FloorEquipmentBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreateFloorequipmentBuilder`</para>Default values. |
GateFeature Class |
Represents a gate feature |
GateFeatureBuilder Class |
Represents a LineDesigner.GateFeature builder |
GlobalSelectionBuilder Class |
Global Selection |
HeadConnectorFeature Class |
Represents a typed connector feature feature |
HoleFeature Class |
Represents a hole feature feature |
HoleFeatureBuilder Class |
Represents a LineDesigner.HoleFeature builder |
ImportFactoryCadGeoBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreateImportFactoryCadGeoBuilder`</para> |
InsertSheet Class |
Represents an insert sheet |
InsertSheetBuilder Class |
Represents a LineDesigner.InsertSheet builder |
JigOnPlaneBuilder Class |
Jig on plane |
LineDesignerApplicationBuilder Class |
Represents a class to create enter and exit the LineDesigner application |
LineDesignerManager Class |
Represents a manager of line designer builders |
ModelBaseObject Class |
Represents Model Base Object |
ModelPlantManager Class |
Represents a manager of line designer model |
ModelPlantRoot Class |
Represents a manager of line designer plant model |
ModelProductionUnit Class |
Represents Production Unit |
ModelResourceInstance Class |
Represents Resource Instance |
PickRectanglePointsBuilder Class |
Pick Rectangle Points |
PlanViewManager Class |
Represents a singleton JA for PlanViewManager |
PlatformEquipmentBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreatePlatformEquipmentBuilder`</para>Default values. |
ProductionUnitCreatorBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreateProductionUnitCreatorBuilder`</para> |
RailOpeningFeature Class |
Represents a rail Opening feature |
RailOpeningFeatureBuilder Class |
Represents a LineDesigner.RailOpeningFeature builder |
RailingFeature Class |
<para>To create or edit an instance of this class, use :py:class:`NXOpen.LineDesigner.RailingFeatureBuilder`</para> |
RailingFeatureBuilder Class |
Represents a LineDesigner.RailingFeature Features. |
RenameItemRevisionBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreateRenameItemRevisionBuilder`</para> |
ResizeConnectorBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreateResizeConnectorBuilder`</para>Default values. |
ReuseLibraryDragData Class |
Represents a manager of line designer plant model |
ReuseLibraryUtilityBuilder Class |
Represents a JA for ReuseLibraryUtility |
SingleElementConveyorBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreateSingleElementConveyorBuilder`</para> |
StairwayEquipmentBuilder Class |
<para>To create a new instance of this class, use :py:meth:`NXOpen.LineDesigner.LineDesignerManager.CreateStairwayEquipmentBuilder`</para>Default values. |
TailConnectorFeature Class |
Represents a typed connector feature feature |
TypedConnectorFeature Class |
Represents a typed connector feature feature |
TypedConnectorFeatureBuilder Class |
Represents a LineDesigner.TypedConnectorFeature Features. |
UINodeUtils Class |
Represents a utils of line designer for journaling uinode methods |