CoverFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
CoverFeatureBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.CoverFeature
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateCoverFeatureBuilder()
Default values.
Property Value CoverThickness.Value 0 (millimeters part), 0 (inches part) LoadRequirements 0 UseCoverOffset 0 New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CoverThickness | Returns the cover thickness |
LoadRequirements | Returns or sets the load requirements |
Tag | Returns the Tag for this object. |
UseCoverOffset | Returns or sets the use cover offset |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CoverThickness¶
-
CoverFeatureBuilder.
CoverThickness
¶ Returns the cover thickness
-------------------------------------
Getter Method
Signature
CoverThickness()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LoadRequirements¶
-
CoverFeatureBuilder.
LoadRequirements
¶ Returns or sets the load requirements
-------------------------------------
Getter Method
Signature
LoadRequirements()
Returns: Return type: float New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
LoadRequirements(loadRequirements)
Parameters: loadRequirements (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UseCoverOffset¶
-
CoverFeatureBuilder.
UseCoverOffset
¶ Returns or sets the use cover offset
-------------------------------------
Getter Method
Signature
UseCoverOffset()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
UseCoverOffset(useCoverOffset)
Parameters: useCoverOffset (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
CoverFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.