CreateFenceBuilder Class¶
-
class
NXOpen.LineDesigner.
CreateFenceBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.CreateFence
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateCreateFenceBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CurveSectionBuilder | Returns the curve section builder |
PostFileBrowser | Returns or sets the post file browser |
SectionFileBrowser | Returns or sets the section file browser |
StartPointPoint | Returns or sets the start point point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CurveSectionBuilder¶
-
CreateFenceBuilder.
CurveSectionBuilder
¶ Returns the curve section builder
-------------------------------------
Getter Method
Signature
CurveSectionBuilder()
Returns: Return type: NXOpen.Section
New in version NX8.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
PostFileBrowser¶
-
CreateFenceBuilder.
PostFileBrowser
¶ Returns or sets the post file browser
-------------------------------------
Getter Method
Signature
PostFileBrowser()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
PostFileBrowser(filename)
Parameters: filename (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SectionFileBrowser¶
-
CreateFenceBuilder.
SectionFileBrowser
¶ Returns or sets the section file browser
-------------------------------------
Getter Method
Signature
SectionFileBrowser()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SectionFileBrowser(filename)
Parameters: filename (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StartPointPoint¶
-
CreateFenceBuilder.
StartPointPoint
¶ Returns or sets the start point point
-------------------------------------
Getter Method
Signature
StartPointPoint()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StartPointPoint(startPointPoint)
Parameters: startPointPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
CreateFenceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.