CreateSystemBuilder Class¶
-
class
NXOpen.LineDesigner.
CreateSystemBuilder
¶ Bases:
NXOpen.Builder
Represents a
LineDesigner.CreateSystem
builderTo create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateCreateSystemBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ArchPartPath | Returns or sets the arch part path |
JigOnPlane | Returns the jig on plane |
LinePartPath | Returns or sets the line part path |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
InitPreview | Do Init Preview. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Update | Do Update. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ArchPartPath¶
-
CreateSystemBuilder.
ArchPartPath
¶ Returns or sets the arch part path
-------------------------------------
Getter Method
Signature
ArchPartPath()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ArchPartPath(filename)
Parameters: filename (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
JigOnPlane¶
-
CreateSystemBuilder.
JigOnPlane
¶ Returns the jig on plane
-------------------------------------
Getter Method
Signature
JigOnPlane()
Returns: Return type: NXOpen.LineDesigner.JigOnPlaneBuilder
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LinePartPath¶
-
CreateSystemBuilder.
LinePartPath
¶ Returns or sets the line part path
-------------------------------------
Getter Method
Signature
LinePartPath()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
LinePartPath(filename)
Parameters: filename (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
InitPreview¶
-
CreateSystemBuilder.
InitPreview
¶ Do Init Preview.
Signature
InitPreview()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Update¶
-
CreateSystemBuilder.
Update
¶ Do Update.
Signature
Update()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
CreateSystemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.