ReuseLibraryDragData Class¶
-
class
NXOpen.LineDesigner.
ReuseLibraryDragData
¶ Bases:
NXOpen.NXObject
Represents a manager of line designer plant model
Established by LineDesigner_ReuseLibraryUtilityBuilder whenever it is needed.
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ActionType | Returns or sets the action type |
CategoryName | Returns or sets the category name |
HasCsysImport | Returns or sets the has csys import |
HasSketchImport | Returns or sets the has sketch import |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
KrxFile | Returns or sets the krx file |
LibName | Returns or sets the lib name |
Name | Returns the custom name of the object. |
NativeItem | Returns or sets the native item |
ObjectId | Returns or sets the object id |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
PartFile | Returns or sets the part file |
PartType | Returns or sets the part type |
PathInLib | Returns or sets the path in lib |
Prototype | Returns the prototype of this object if it is an occurrence. |
SpareDialogForDragAndDrop | Returns or sets the spare dialog for drag and drop |
Tag | Returns the Tag for this object. |
TemplateName | Returns or sets the template name |
TypeName | Returns or sets the type name |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
ActionType¶
-
ReuseLibraryDragData.
ActionType
¶ Returns or sets the action type
-------------------------------------
Getter Method
Signature
ActionType()
Returns: Return type: int New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ActionType(actionType)
Parameters: actionType (int) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
CategoryName¶
-
ReuseLibraryDragData.
CategoryName
¶ Returns or sets the category name
-------------------------------------
Getter Method
Signature
CategoryName()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
CategoryName(categoryName)
Parameters: categoryName (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
HasCsysImport¶
-
ReuseLibraryDragData.
HasCsysImport
¶ Returns or sets the has csys import
-------------------------------------
Getter Method
Signature
HasCsysImport()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
HasCsysImport(hasCsysImport)
Parameters: hasCsysImport (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
HasSketchImport¶
-
ReuseLibraryDragData.
HasSketchImport
¶ Returns or sets the has sketch import
-------------------------------------
Getter Method
Signature
HasSketchImport()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
HasSketchImport(hasSketchImport)
Parameters: hasSketchImport (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
IsOccurrence¶
-
ReuseLibraryDragData.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
ReuseLibraryDragData.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
KrxFile¶
-
ReuseLibraryDragData.
KrxFile
¶ Returns or sets the krx file
-------------------------------------
Getter Method
Signature
KrxFile()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
KrxFile(krxFile)
Parameters: krxFile (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
LibName¶
-
ReuseLibraryDragData.
LibName
¶ Returns or sets the lib name
-------------------------------------
Getter Method
Signature
LibName()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
LibName(libName)
Parameters: libName (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Name¶
-
ReuseLibraryDragData.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
NativeItem¶
-
ReuseLibraryDragData.
NativeItem
¶ Returns or sets the native item
-------------------------------------
Getter Method
Signature
NativeItem()
Returns: Return type: int New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
NativeItem(nativeItem)
Parameters: nativeItem (int) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ObjectId¶
-
ReuseLibraryDragData.
ObjectId
¶ Returns or sets the object id
-------------------------------------
Getter Method
Signature
ObjectId()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ObjectId(objectId)
Parameters: objectId (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
OwningComponent¶
-
ReuseLibraryDragData.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
ReuseLibraryDragData.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
PartFile¶
-
ReuseLibraryDragData.
PartFile
¶ Returns or sets the part file
-------------------------------------
Getter Method
Signature
PartFile()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
PartFile(partFile)
Parameters: partFile (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
PartType¶
-
ReuseLibraryDragData.
PartType
¶ Returns or sets the part type
-------------------------------------
Getter Method
Signature
PartType()
Returns: Return type: int New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
PartType(partType)
Parameters: partType (int) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
PathInLib¶
-
ReuseLibraryDragData.
PathInLib
¶ Returns or sets the path in lib
-------------------------------------
Getter Method
Signature
PathInLib()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
PathInLib(pathInLib)
Parameters: pathInLib (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Prototype¶
-
ReuseLibraryDragData.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
SpareDialogForDragAndDrop¶
-
ReuseLibraryDragData.
SpareDialogForDragAndDrop
¶ Returns or sets the spare dialog for drag and drop
-------------------------------------
Getter Method
Signature
SpareDialogForDragAndDrop()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SpareDialogForDragAndDrop(spareDialogForDragAndDrop)
Parameters: spareDialogForDragAndDrop (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
TemplateName¶
-
ReuseLibraryDragData.
TemplateName
¶ Returns or sets the template name
-------------------------------------
Getter Method
Signature
TemplateName()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
TemplateName(templateName)
Parameters: templateName (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
TypeName¶
-
ReuseLibraryDragData.
TypeName
¶ Returns or sets the type name
-------------------------------------
Getter Method
Signature
TypeName()
Returns: Return type: str New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
TypeName(typeName)
Parameters: typeName (str) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
FindObject¶
-
ReuseLibraryDragData.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
ReuseLibraryDragData.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
ReuseLibraryDragData.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.