PlatformEquipmentBuilder Class¶
-
class
NXOpen.LineDesigner.
PlatformEquipmentBuilder
¶ Bases:
NXOpen.Builder
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreatePlatformEquipmentBuilder()
Default values.
Property Value AddRailingToggle 1 DeckCeilingHeightForCenterline.Value 9000 (millimeters part), 354.5 (inches part) DeckCeilingHeightForPolyline.Value 9000 (millimeters part), 354.5 (inches part) DeckElevationForCenterline.Value 0 (millimeters part), 0 (inches part) DeckElevationForPolyline.Value 0 (millimeters part), 0 (inches part) DeckHeightForCenterline.Value 525 (millimeters part), 21 (inches part) DeckHeightForPolyline.Value 1750 (millimeters part), 68.9 (inches part) DeckLengthForCenterline.Value 2540 (millimeters part), 100 (inches part) DeckSupportEnum NoSupports DeckThicknessForCenterline.Value 300 (millimeters part), 12 (inches part) DeckThicknessForPolyline.Value 300 (millimeters part), 12 (inches part) DeckWidthForCenterline.Value 2438 (millimeters part), 96 (inches part) DeckingMaterial MetalGrate DistanceFromCenterline.Value 660 (millimeters part), 26 (inches part) HorizontalGridSpacing.Value 4000 (millimeters part), 157.5 (inches part) OutlineEnum Polyline SideFromCenterlineEnum RightTopSide SupportsFromCeiling 0 TypeEnum Platform VerticalGridSpacing.Value 3200 (millimeters part), 126 (inches part) New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AddRailingToggle | Returns or sets the add railing toggle |
CenterlineJigOnPlane | Returns or sets the centerline jig on plane |
DeckCeilingHeightForCenterline | Returns the deck ceiling height for centerline |
DeckCeilingHeightForPolyline | Returns the deck ceiling height for polyline |
DeckElevationForCenterline | Returns the deck elevation for centerline |
DeckElevationForPolyline | Returns the deck elevation for polyline |
DeckHeightForCenterline | Returns the deck height for centerline |
DeckHeightForPolyline | Returns the deck height for polyline |
DeckLengthForCenterline | Returns the deck length for centerline |
DeckSupportEnum | Returns or sets the deck support enum |
DeckThicknessForCenterline | Returns the deck thickness for centerline |
DeckThicknessForPolyline | Returns the deck thickness for polyline |
DeckWidthForCenterline | Returns the deck width for centerline |
DeckingMaterial | Returns or sets the decking material |
DistanceFromCenterline | Returns the distance from centerline |
HorizontalGridSpacing | Returns the horizontal grid spacing |
IsSketchInternal | Returns or sets the issketchiInternal |
KfObject | Returns the kf object |
OutlineEnum | Returns or sets the outline enum |
PolylineSuperSection | Returns the polyline super section |
SideFromCenterlineEnum | Returns or sets the side from centerline enum |
StatusOfPlatformCeilingHeightUpdation | Returns or sets the platform ceiling height updation status |
StatusOfPlatformElevationUpdation | Returns or sets the platform elevation updation status |
StatusOfPlatformHeightUpdation | Returns or sets the platform height updation status |
StatusOfPlatformSupportDefaultFromCeilingToggleUpdation | Returns or sets the platform supportDefaultFromCeilingToggle updation status |
StatusOfPlatformSupportOptionUpdation | Returns or sets the platform supportOption updation status |
StatusOfPlatformThicknessUpdation | Returns or sets the platform thickness updation status |
SupportsFromCeiling | Returns or sets the supports from ceiling |
Tag | Returns the Tag for this object. |
TypeEnum | Returns or sets the type enum |
VerticalGridSpacing | Returns the vertical grid spacing |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
SupportCrossSectionButton | TODO: fill in a description for this |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
Property Detail¶
AddRailingToggle¶
-
PlatformEquipmentBuilder.
AddRailingToggle
¶ Returns or sets the add railing toggle
-------------------------------------
Getter Method
Signature
AddRailingToggle()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
AddRailingToggle(addRailingToggle)
Parameters: addRailingToggle (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
CenterlineJigOnPlane¶
-
PlatformEquipmentBuilder.
CenterlineJigOnPlane
¶ Returns or sets the centerline jig on plane
-------------------------------------
Getter Method
Signature
CenterlineJigOnPlane()
Returns: Return type: NXOpen.LineDesigner.JigOnPlaneBuilder
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
CenterlineJigOnPlane(centerlineJigOnPlane)
Parameters: centerlineJigOnPlane ( NXOpen.LineDesigner.JigOnPlaneBuilder
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckCeilingHeightForCenterline¶
-
PlatformEquipmentBuilder.
DeckCeilingHeightForCenterline
¶ Returns the deck ceiling height for centerline
-------------------------------------
Getter Method
Signature
DeckCeilingHeightForCenterline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckCeilingHeightForPolyline¶
-
PlatformEquipmentBuilder.
DeckCeilingHeightForPolyline
¶ Returns the deck ceiling height for polyline
-------------------------------------
Getter Method
Signature
DeckCeilingHeightForPolyline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckElevationForCenterline¶
-
PlatformEquipmentBuilder.
DeckElevationForCenterline
¶ Returns the deck elevation for centerline
-------------------------------------
Getter Method
Signature
DeckElevationForCenterline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckElevationForPolyline¶
-
PlatformEquipmentBuilder.
DeckElevationForPolyline
¶ Returns the deck elevation for polyline
-------------------------------------
Getter Method
Signature
DeckElevationForPolyline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckHeightForCenterline¶
-
PlatformEquipmentBuilder.
DeckHeightForCenterline
¶ Returns the deck height for centerline
-------------------------------------
Getter Method
Signature
DeckHeightForCenterline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckHeightForPolyline¶
-
PlatformEquipmentBuilder.
DeckHeightForPolyline
¶ Returns the deck height for polyline
-------------------------------------
Getter Method
Signature
DeckHeightForPolyline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckLengthForCenterline¶
-
PlatformEquipmentBuilder.
DeckLengthForCenterline
¶ Returns the deck length for centerline
-------------------------------------
Getter Method
Signature
DeckLengthForCenterline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckSupportEnum¶
-
PlatformEquipmentBuilder.
DeckSupportEnum
¶ Returns or sets the deck support enum
-------------------------------------
Getter Method
Signature
DeckSupportEnum()
Returns: Return type: NXOpen.LineDesigner.PlatformEquipmentBuilderDeckSupportTypeAPI
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
DeckSupportEnum(deckSupportEnum)
Parameters: deckSupportEnum ( NXOpen.LineDesigner.PlatformEquipmentBuilderDeckSupportTypeAPI
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckThicknessForCenterline¶
-
PlatformEquipmentBuilder.
DeckThicknessForCenterline
¶ Returns the deck thickness for centerline
-------------------------------------
Getter Method
Signature
DeckThicknessForCenterline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckThicknessForPolyline¶
-
PlatformEquipmentBuilder.
DeckThicknessForPolyline
¶ Returns the deck thickness for polyline
-------------------------------------
Getter Method
Signature
DeckThicknessForPolyline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckWidthForCenterline¶
-
PlatformEquipmentBuilder.
DeckWidthForCenterline
¶ Returns the deck width for centerline
-------------------------------------
Getter Method
Signature
DeckWidthForCenterline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DeckingMaterial¶
-
PlatformEquipmentBuilder.
DeckingMaterial
¶ Returns or sets the decking material
-------------------------------------
Getter Method
Signature
DeckingMaterial()
Returns: Return type: NXOpen.LineDesigner.PlatformEquipmentBuilderDeckingMaterialTypeAPI
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
DeckingMaterial(deckingMaterial)
Parameters: deckingMaterial ( NXOpen.LineDesigner.PlatformEquipmentBuilderDeckingMaterialTypeAPI
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
DistanceFromCenterline¶
-
PlatformEquipmentBuilder.
DistanceFromCenterline
¶ Returns the distance from centerline
-------------------------------------
Getter Method
Signature
DistanceFromCenterline()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
HorizontalGridSpacing¶
-
PlatformEquipmentBuilder.
HorizontalGridSpacing
¶ Returns the horizontal grid spacing
-------------------------------------
Getter Method
Signature
HorizontalGridSpacing()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
IsSketchInternal¶
-
PlatformEquipmentBuilder.
IsSketchInternal
¶ Returns or sets the issketchiInternal
-------------------------------------
Getter Method
Signature
IsSketchInternal()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
IsSketchInternal(makeSketchInternal)
Parameters: makeSketchInternal (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
KfObject¶
-
PlatformEquipmentBuilder.
KfObject
¶ Returns the kf object
-------------------------------------
Getter Method
Signature
KfObject()
Returns: Return type: NXOpen.KFObject
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
OutlineEnum¶
-
PlatformEquipmentBuilder.
OutlineEnum
¶ Returns or sets the outline enum
-------------------------------------
Getter Method
Signature
OutlineEnum()
Returns: Return type: NXOpen.LineDesigner.PlatformEquipmentBuilderOutlineTypeAPI
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
OutlineEnum(outlineEnum)
Parameters: outlineEnum ( NXOpen.LineDesigner.PlatformEquipmentBuilderOutlineTypeAPI
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
PolylineSuperSection¶
-
PlatformEquipmentBuilder.
PolylineSuperSection
¶ Returns the polyline super section
-------------------------------------
Getter Method
Signature
PolylineSuperSection()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SideFromCenterlineEnum¶
-
PlatformEquipmentBuilder.
SideFromCenterlineEnum
¶ Returns or sets the side from centerline enum
-------------------------------------
Getter Method
Signature
SideFromCenterlineEnum()
Returns: Return type: NXOpen.LineDesigner.PlatformEquipmentBuilderSideFromCenterlineTypeAPI
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SideFromCenterlineEnum(sideFromCenterlineEnum)
Parameters: sideFromCenterlineEnum ( NXOpen.LineDesigner.PlatformEquipmentBuilderSideFromCenterlineTypeAPI
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StatusOfPlatformCeilingHeightUpdation¶
-
PlatformEquipmentBuilder.
StatusOfPlatformCeilingHeightUpdation
¶ Returns or sets the platform ceiling height updation status
-------------------------------------
Getter Method
Signature
StatusOfPlatformCeilingHeightUpdation()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StatusOfPlatformCeilingHeightUpdation(statusOfPlatformCeilingHeightUpdation)
Parameters: statusOfPlatformCeilingHeightUpdation (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StatusOfPlatformElevationUpdation¶
-
PlatformEquipmentBuilder.
StatusOfPlatformElevationUpdation
¶ Returns or sets the platform elevation updation status
-------------------------------------
Getter Method
Signature
StatusOfPlatformElevationUpdation()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StatusOfPlatformElevationUpdation(statusOfPlatformElevationUpdation)
Parameters: statusOfPlatformElevationUpdation (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StatusOfPlatformHeightUpdation¶
-
PlatformEquipmentBuilder.
StatusOfPlatformHeightUpdation
¶ Returns or sets the platform height updation status
-------------------------------------
Getter Method
Signature
StatusOfPlatformHeightUpdation()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StatusOfPlatformHeightUpdation(statusOfPlatformHeightUpdation)
Parameters: statusOfPlatformHeightUpdation (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StatusOfPlatformSupportDefaultFromCeilingToggleUpdation¶
-
PlatformEquipmentBuilder.
StatusOfPlatformSupportDefaultFromCeilingToggleUpdation
¶ Returns or sets the platform supportDefaultFromCeilingToggle updation status
-------------------------------------
Getter Method
Signature
StatusOfPlatformSupportDefaultFromCeilingToggleUpdation()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StatusOfPlatformSupportDefaultFromCeilingToggleUpdation(statusOfPlatformSupportDefaultFromCeilingToggleUpdation)
Parameters: statusOfPlatformSupportDefaultFromCeilingToggleUpdation (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StatusOfPlatformSupportOptionUpdation¶
-
PlatformEquipmentBuilder.
StatusOfPlatformSupportOptionUpdation
¶ Returns or sets the platform supportOption updation status
-------------------------------------
Getter Method
Signature
StatusOfPlatformSupportOptionUpdation()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StatusOfPlatformSupportOptionUpdation(statusOfPlatformSupportOptionUpdation)
Parameters: statusOfPlatformSupportOptionUpdation (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
StatusOfPlatformThicknessUpdation¶
-
PlatformEquipmentBuilder.
StatusOfPlatformThicknessUpdation
¶ Returns or sets the platform thickness updation status
-------------------------------------
Getter Method
Signature
StatusOfPlatformThicknessUpdation()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
StatusOfPlatformThicknessUpdation(statusOfPlatformThicknessUpdation)
Parameters: statusOfPlatformThicknessUpdation (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SupportsFromCeiling¶
-
PlatformEquipmentBuilder.
SupportsFromCeiling
¶ Returns or sets the supports from ceiling
-------------------------------------
Getter Method
Signature
SupportsFromCeiling()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
SupportsFromCeiling(supportsFromCeiling)
Parameters: supportsFromCeiling (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
TypeEnum¶
-
PlatformEquipmentBuilder.
TypeEnum
¶ Returns or sets the type enum
-------------------------------------
Getter Method
Signature
TypeEnum()
Returns: Return type: NXOpen.LineDesigner.PlatformEquipmentBuilderTypeAPI
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
TypeEnum(typeEnum)
Parameters: typeEnum ( NXOpen.LineDesigner.PlatformEquipmentBuilderTypeAPI
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
VerticalGridSpacing¶
-
PlatformEquipmentBuilder.
VerticalGridSpacing
¶ Returns the vertical grid spacing
-------------------------------------
Getter Method
Signature
VerticalGridSpacing()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
SupportCrossSectionButton¶
-
PlatformEquipmentBuilder.
SupportCrossSectionButton
¶ TODO: fill in a description for this
Signature
SupportCrossSectionButton()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
PlatformEquipmentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.