DBNodeNodeType Enumeration

NXOpen.LineDesigner.DBNode.NodeType is an alias for NXOpen.LineDesigner.DBNodeNodeType

class NXOpen.LineDesigner.DBNodeNodeType

Bases: object

Define the node type

Enum Members

Enum Member Enum Member Description
Factory
Fence
PlatformEquipment
Conveyor
FloorEquipment
ColumnGridEquipment
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.