ExportPlantToDWGBuilderSaveAsType Enumeration

NXOpen.LineDesigner.ExportPlantToDWGBuilder.SaveAsType is an alias for NXOpen.LineDesigner.ExportPlantToDWGBuilderSaveAsType

class NXOpen.LineDesigner.ExportPlantToDWGBuilderSaveAsType

Bases: object

Represents the dwg saving types

Enum Members

Enum Member Enum Member Description
T2d
Represents the 2D type
T3d
Represents the 3D type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.