InsertSheetBuilderAPIUnits Enumeration

NXOpen.LineDesigner.InsertSheetBuilder.APIUnits is an alias for NXOpen.LineDesigner.InsertSheetBuilderAPIUnits

class NXOpen.LineDesigner.InsertSheetBuilderAPIUnits

Bases: object

Represents the units types

Enum Members

Enum Member Enum Member Description
Millimeters
Represents the Millimeters type
Inches
Represents the Inches type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.