CreateFactoryElementBuilderTypeAPI Enumeration¶
NXOpen.LineDesigner.CreateFactoryElementBuilder.TypeAPI is an alias for NXOpen.LineDesigner.CreateFactoryElementBuilderTypeAPI
-
class
NXOpen.LineDesigner.
CreateFactoryElementBuilderTypeAPI
¶ Bases:
object
Represents the factory element types
Enum Members
Enum Member Enum Member Description Plant Represents the Plant typeStation Represents the Station typeLine Represents the Line typeZone Represents the Zone typePartition Represents the Partition type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-