DBFactoryNodeNodeType Enumeration

NXOpen.LineDesigner.DBFactoryNode.NodeType is an alias for NXOpen.LineDesigner.DBFactoryNodeNodeType

class NXOpen.LineDesigner.DBFactoryNodeNodeType

Bases: object

Define the factory node type

Enum Members

Enum Member Enum Member Description
Plant
Station
Line
Zone
Partition
Unknown
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.