ColumnGridEquipmentBuilderColumnType Enumeration

NXOpen.LineDesigner.ColumnGridEquipmentBuilder.ColumnType is an alias for NXOpen.LineDesigner.ColumnGridEquipmentBuilderColumnType

class NXOpen.LineDesigner.ColumnGridEquipmentBuilderColumnType

Bases: object

Enum Members

Enum Member Enum Member Description
IBeam
TBeam
Rectangle
Circle
UserDefine
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.