ColumnFeatureBuilder Class¶
-
class
NXOpen.LineDesigner.
ColumnFeatureBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
LineDesigner.ColumnFeature
Features.FeatureBuilder
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreateColumnFeatureBuilder()
Default values.
Property Value BaseDepth.Value 800 (millimeters part), 32 (inches part) BaseDiameter.Value 800 (millimeters part), 32 (inches part) BaseHeight.Value 900 (millimeters part), 35 (inches part) BaseLowerDiameter.Value 900 (millimeters part), 35 (inches part) BaseStyleEnum None BaseUpperDiameter.Value 800 (millimeters part), 32 (inches part) BaseWidth.Value 800 (millimeters part), 32 (inches part) ColumnDepth.Value 600 (millimeters part), 25 (inches part) ColumnDiameter.Value 300 (millimeters part), 12 (inches part) ColumnHeight.Value 3000 (millimeters part), 120 (inches part) ColumnStyleEnum IBeam ColumnThickness.Value 30 (millimeters part), 2 (inches part) ColumnWidth.Value 600 (millimeters part), 25 (inches part) New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
BaseDepth | Returns the base depth |
BaseDiameter | Returns the base diameter |
BaseHeight | Returns the base height |
BaseLowerDiameter | Returns the base lower diameter |
BaseStyleEnum | Returns or sets the base style enum |
BaseUpperDiameter | Returns the base upper diameter |
BaseUserDefineSuperSection | Returns the base user define super section |
BaseWidth | Returns the base width |
ColumnDepth | Returns the column depth |
ColumnDiameter | Returns the column diameter |
ColumnHeight | Returns the column height |
ColumnOriginPoint | Returns or sets the column origin point |
ColumnStyleEnum | Returns or sets the column style enum |
ColumnThickness | Returns the column thickness |
ColumnUserDefineSuperSection | Returns the column user define super section |
ColumnWidth | Returns the column width |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ShouldCopySketchBase | Returns or sets |
ShouldCopySketchColumn | Returns or sets |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ColumnFeatureBuilderColumnBaseType Enumeration | |
ColumnFeatureBuilderColumnType Enumeration |
Property Detail¶
BaseDepth¶
-
ColumnFeatureBuilder.
BaseDepth
¶ Returns the base depth
-------------------------------------
Getter Method
Signature
BaseDepth()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseDiameter¶
-
ColumnFeatureBuilder.
BaseDiameter
¶ Returns the base diameter
-------------------------------------
Getter Method
Signature
BaseDiameter()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseHeight¶
-
ColumnFeatureBuilder.
BaseHeight
¶ Returns the base height
-------------------------------------
Getter Method
Signature
BaseHeight()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseLowerDiameter¶
-
ColumnFeatureBuilder.
BaseLowerDiameter
¶ Returns the base lower diameter
-------------------------------------
Getter Method
Signature
BaseLowerDiameter()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseStyleEnum¶
-
ColumnFeatureBuilder.
BaseStyleEnum
¶ Returns or sets the base style enum
-------------------------------------
Getter Method
Signature
BaseStyleEnum()
Returns: Return type: NXOpen.LineDesigner.ColumnFeatureBuilderColumnBaseType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
BaseStyleEnum(baseStyleEnum)
Parameters: baseStyleEnum ( NXOpen.LineDesigner.ColumnFeatureBuilderColumnBaseType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseUpperDiameter¶
-
ColumnFeatureBuilder.
BaseUpperDiameter
¶ Returns the base upper diameter
-------------------------------------
Getter Method
Signature
BaseUpperDiameter()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseUserDefineSuperSection¶
-
ColumnFeatureBuilder.
BaseUserDefineSuperSection
¶ Returns the base user define super section
-------------------------------------
Getter Method
Signature
BaseUserDefineSuperSection()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
BaseWidth¶
-
ColumnFeatureBuilder.
BaseWidth
¶ Returns the base width
-------------------------------------
Getter Method
Signature
BaseWidth()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnDepth¶
-
ColumnFeatureBuilder.
ColumnDepth
¶ Returns the column depth
-------------------------------------
Getter Method
Signature
ColumnDepth()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnDiameter¶
-
ColumnFeatureBuilder.
ColumnDiameter
¶ Returns the column diameter
-------------------------------------
Getter Method
Signature
ColumnDiameter()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnHeight¶
-
ColumnFeatureBuilder.
ColumnHeight
¶ Returns the column height
-------------------------------------
Getter Method
Signature
ColumnHeight()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnOriginPoint¶
-
ColumnFeatureBuilder.
ColumnOriginPoint
¶ Returns or sets the column origin point
-------------------------------------
Getter Method
Signature
ColumnOriginPoint()
Returns: Return type: NXOpen.Point
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ColumnOriginPoint(columnOriginPoint)
Parameters: columnOriginPoint ( NXOpen.Point
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnStyleEnum¶
-
ColumnFeatureBuilder.
ColumnStyleEnum
¶ Returns or sets the column style enum
-------------------------------------
Getter Method
Signature
ColumnStyleEnum()
Returns: Return type: NXOpen.LineDesigner.ColumnFeatureBuilderColumnType
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ColumnStyleEnum(columnStyleEnum)
Parameters: columnStyleEnum ( NXOpen.LineDesigner.ColumnFeatureBuilderColumnType
) –New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnThickness¶
-
ColumnFeatureBuilder.
ColumnThickness
¶ Returns the column thickness
-------------------------------------
Getter Method
Signature
ColumnThickness()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnUserDefineSuperSection¶
-
ColumnFeatureBuilder.
ColumnUserDefineSuperSection
¶ Returns the column user define super section
-------------------------------------
Getter Method
Signature
ColumnUserDefineSuperSection()
Returns: Return type: NXOpen.Section
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ColumnWidth¶
-
ColumnFeatureBuilder.
ColumnWidth
¶ Returns the column width
-------------------------------------
Getter Method
Signature
ColumnWidth()
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ShouldCopySketchBase¶
-
ColumnFeatureBuilder.
ShouldCopySketchBase
¶ Returns or sets
-------------------------------------
Getter Method
Signature
ShouldCopySketchBase()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ShouldCopySketchBase(shouldCopySketchBase)
Parameters: shouldCopySketchBase (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ShouldCopySketchColumn¶
-
ColumnFeatureBuilder.
ShouldCopySketchColumn
¶ Returns or sets
-------------------------------------
Getter Method
Signature
ShouldCopySketchColumn()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
ShouldCopySketchColumn(shouldCopySketchColumn)
Parameters: shouldCopySketchColumn (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
Validate¶
-
ColumnFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.