ConveyorStationFeatureBuilderType Enumeration

NXOpen.LineDesigner.ConveyorStationFeatureBuilder.Type is an alias for NXOpen.LineDesigner.ConveyorStationFeatureBuilderType

class NXOpen.LineDesigner.ConveyorStationFeatureBuilderType

Bases: object

Enum Members

Enum Member Enum Member Description
Load
Unload
ProcessRun
ProcessStop
Idle
Decision
Marriage
Disassembly
Assembly
Stop
LimitSwitch
ProximitySwitch
Reader
Pusher
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.