PickRectanglePointsBuilder Class¶
-
class
NXOpen.LineDesigner.
PickRectanglePointsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Pick Rectangle Points
To create a new instance of this class, use
NXOpen.LineDesigner.LineDesignerManager.CreatePickRectanglePointsBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AllowRotation | Returns or sets the rotaion |
PointsSelection | Returns the pointsSelection |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ResetData | ResetData |
ResetWidthHeight | ResetWidthHeight |
SetWidthHeight | SetWidthHeight |
UpdateRecAngle | UpdateRecAngle |
UpdateRecHeight | UpdateRecHeight |
UpdateRecWidth | UpdateRecWidth |
UpdateRectangle | UpdateRectangle |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AllowRotation¶
-
PickRectanglePointsBuilder.
AllowRotation
¶ Returns or sets the rotaion
-------------------------------------
Getter Method
Signature
AllowRotation()
Returns: Return type: bool New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
-------------------------------------
Setter Method
Signature
AllowRotation(rotaion)
Parameters: rotaion (bool) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
PointsSelection¶
-
PickRectanglePointsBuilder.
PointsSelection
¶ Returns the pointsSelection
-------------------------------------
Getter Method
Signature
PointsSelection()
Returns: Return type: NXOpen.SelectPartList
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Method Detail¶
ResetData¶
-
PickRectanglePointsBuilder.
ResetData
¶ Signature
ResetData()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
ResetWidthHeight¶
-
PickRectanglePointsBuilder.
ResetWidthHeight
¶ Signature
ResetWidthHeight()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
SetWidthHeight¶
-
PickRectanglePointsBuilder.
SetWidthHeight
¶ Signature
SetWidthHeight(width, height)
Parameters: - width (float) –
- height (float) –
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UpdateRecAngle¶
-
PickRectanglePointsBuilder.
UpdateRecAngle
¶ Signature
UpdateRecAngle(angle)
Parameters: angle (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UpdateRecHeight¶
-
PickRectanglePointsBuilder.
UpdateRecHeight
¶ Signature
UpdateRecHeight(height)
Parameters: height (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UpdateRecWidth¶
-
PickRectanglePointsBuilder.
UpdateRecWidth
¶ Signature
UpdateRecWidth(width)
Parameters: width (float) – New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
UpdateRectangle¶
-
PickRectanglePointsBuilder.
UpdateRectangle
¶ Signature
UpdateRectangle()
New in version NX9.0.0.
License requirements: ld_line_designer (“FULL LINE DESIGNER”)
Validate¶
-
PickRectanglePointsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.